How can I use Bluetooth speaker in imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I use Bluetooth speaker in imx6

1,322 次查看
titusstalin
Contributor V

Hello Experts,

Want to play an audio file in BT speaker using imx6 board.

I have installed the pulseaudio and don't know how to use.

Also I have installed the bluez and bluetoothctl, able to up the Bluetooth in imx6 board and able to see the nearest BT speaker device.

But pacmd and pactl command outputs not showing the sink and source devices of BT speaker and bluez stack.

 

root@imx6:~#
root@imx6:~#
root@imx6:~# pulseaudio
W: [pulseaudio] main.c: This program is not intended to be run as root (unless --system is specified).

 

root@imx6:~#
root@imx6:~#
root@-imx6:/#
root@-imx6:/# bluetoothctl
[NEW] Controller 00:19:86:00:1E:B6 bt-imx6 [default]
[NEW] Device 00:E0:4C:C5:64:61 SoundCore mini(ATT)
[bluetooth]#

 

Attached the log.

Am I missing any configuration ?

Can you please help me ?

 

Regards,

Titus S.

Original Attachment has been moved to: pacmd_pactl_outputs.txt.zip

标签 (3)
0 项奖励
回复
1 回复

902 次查看
diegoadrian
NXP Employee
NXP Employee

Hello Titus,

Do you know if your bluetooth driver can be used with bluez and bluetoothctl.

Best Regards,

Diego.

0 项奖励
回复