Hello Experts,
Want to play an audio file in BT speaker using imx6 board.
I have installed the pulseaudio and don't know how to use.
Also I have installed the bluez and bluetoothctl, able to up the Bluetooth in imx6 board and able to see the nearest BT speaker device.
But pacmd and pactl command outputs not showing the sink and source devices of BT speaker and bluez stack.
root@imx6:~#
root@imx6:~#
root@imx6:~# pulseaudio
W: [pulseaudio] main.c: This program is not intended to be run as root (unless --system is specified).
root@imx6:~#
root@imx6:~#
root@-imx6:/#
root@-imx6:/# bluetoothctl
[NEW] Controller 00:19:86:00:1E:B6 bt-imx6 [default]
[NEW] Device 00:E0:4C:C5:64:61 SoundCore mini(ATT)
[bluetooth]#
Attached the log.
Am I missing any configuration ?
Can you please help me ?
Regards,
Titus S.
Original Attachment has been moved to: pacmd_pactl_outputs.txt.zip