igorpadykov 留言:
Hi tsung
one can migrate to Linux 4.9.11, it uses Qt5.8 as described in
sect.2.1 New features attached Release Notes.
Linux 4.9.11_1.0.0 BSP & Multimedia Codecs Documentation
https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061...
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your reply.
I'm wondering what is the difference between fsl-image-qt5 and fsl-image-validation-qt5-imx?
As the i.MX Yocto Project User's Guide document showed, I should l build fsl-image-validation-qt5-imx to have my QT5 image and using hardware graphics.
But in fsl-yocto_L4.9.11_1.0.0 folder there is a README file, it said you could build image with fsl-image-gui or fsl-image-qt5 to have fsl-image-gui with QT 5.8.
I can tell the difference between fsl-image-qt5 and fsl-image-validation-qt5-imx.
Which is more proper in my condition?