How can I set 854x480 parallel LCD panel ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I set 854x480 parallel LCD panel ?

2,384 次查看
leeinchul
Contributor II

Hi, all.

I want to set 854x480 parallel LCD panel. So, I set parameters as the below.

1. Is it correcting set?

2. I cannot understand variables, ".interface_pix_fmt", "default_bpp". Would you give me some information about this

Thanks and best regards.

.................................................................................................................................

[u-boot]

bootargs_nfs_rgb24=setenv bootargs ${bootargs_base} root=/dev/nfs ip=${ipaddr}:${gatewayip}:${netmask}:${hostname}:eth0::off rw nfsroot=${serverip}:${rootpath},v3,tcp video=mxcfb0:dev=lcd,ARHUD-PGU,if=RGB24 video=mxcfb1:off video=mxcfb2:off

[board_mx6q_sabreauto.c]

static struct ipuv3_fb_platform_data sabr_fb_data[] = {

{ /*fb0*/

  .disp_dev           = "lcd",

  .interface_pix_fmt  = IPU_PIX_FMT_RGB24,

  .mode_str           = "ARHUD-PGU",

  .default_bpp        = 16,

  .int_clk            = false,

},{ /*fb1*/

  .disp_dev  = "ldb",

  .interface_pix_fmt = IPU_PIX_FMT_RGB666,

  .mode_str  = "LDB-XGA",

  .default_bpp  = 16,

  .int_clk  = false,

}, { /*fb2*/

  .disp_dev  = "ldb",

  .interface_pix_fmt = IPU_PIX_FMT_RGB666,

  .mode_str  = "LDB-XGA",

  .default_bpp  = 16,

  .int_clk  = false,

},

};

[mxc_lcdif.c]

static struct fb_videomode lcdif_modedb[] = {

{

/* 800x480 @ 57 Hz , pixel clk @ 27MHz */

"CLAA-WVGA", 57, 800, 480, 37037, 40, 60, 10, 10, 20, 10,

FB_SYNC_CLK_LAT_FALL,

FB_VMODE_NONINTERLACED,

0,},

{

/* 800x480 @ 60 Hz , pixel clk @ 32MHz */

"SEIKO-WVGA", 60, 800, 480, 29850, 89, 164, 23, 10, 10, 10,

FB_SYNC_CLK_LAT_FALL,

FB_VMODE_NONINTERLACED,

0,},

{

/* 854x480 @ 60 Hz , pixel clk @ 32MHz */

"ARHUD-PGU", 60, 854, 480, 29850, 89, 164, 23, 10, 10, 10,

FB_SYNC_CLK_LAT_FALL,

FB_VMODE_NONINTERLACED,

0,},

};

标签 (3)
标记 (2)
0 项奖励
回复
4 回复数

1,806 次查看
Yuri
NXP Employee
NXP Employee

   You may look at app note AN3974 “Different Display Configurations on

i.MX35 Linux PDK” regarding Linux framebuffer structures.

http://cache.freescale.com/files/dsp/doc/app_note/AN3974.pdf


“interface_pix_fmt" -  defines format of memory, reserved for pixel. 

"default_bpp" – default bits per pixel  parameter.

Have a great day,

Yuri

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,806 次查看
eugenevolkov
Contributor IV

Hi, Yuri!

I configure parallel LCD in my board. I use 3.10.53_1.1.0-ga relise.

But, i not find board_mx6q_sabreauto.c file

May meant the mx6q_sabreauto.dtsi file?



0 项奖励
回复

1,806 次查看
Yuri
NXP Employee
NXP Employee

Yes,

  "For the i.MX 6Quad/6DualLite/6SoloLite/6SoloX, the board specific
configuration options for the driver are set in:

arch/arm/boot/dts/imx6*.dtsi

arch/arm/boot/dts/imx6*.dts"

Regards,

Yuri.

0 项奖励
回复

1,806 次查看
leeinchul
Contributor II

Hi, Yuri.

Thank you for your reference.

Have a nice day.

Inchul.

0 项奖励
回复