Hi NXP Tech Team,
I'm using i.MX 8QuadMax MEK with L5.4.70 kernel image.
Could you tell me the way to set 56 pin of M.2 connector to High?
I think it's need to set LVDS1_I2C0_SDA of MIMX8QM6AVUFFAB to High(1.8V), but I don't know the way.
Regards,
解決済! 解決策の投稿を見る。
Hello,
I would like to know what are you trying to achieve since this pad is already defined in default device tree:
https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.d...
https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.d...
Also:
https://source.codeaurora.org/external/imx/linux-imx/commit/?h=imx_5.4.70_2.3.0&id=764a31f31823776c7...
Best regards,
Aldo.
Hi Aldo
Sorry for my late response.
I confirmed whethre the 56 pin is High with the image which included my changes.
So I re-confirmed it with the image which didn't incluede my changes and I could confirm that the pin is High.
Thank you for your support.
Best Regards,
Shinya
Hello,
I would like to know what are you trying to achieve since this pad is already defined in default device tree:
https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.d...
https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8qm-mek.d...
Also:
https://source.codeaurora.org/external/imx/linux-imx/commit/?h=imx_5.4.70_2.3.0&id=764a31f31823776c7...
Best regards,
Aldo.