How can I output sound simultaneously to the hdmi sound and the internal sound of Imx6q?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I output sound simultaneously to the hdmi sound and the internal sound of Imx6q?

Jump to solution
1,820 Views
jongjupark
Contributor I

Dear community,

How can I output sound simultaneously to the hdmi sound and the internal sound of Imx6q?

Is there a hdmi sound source to write i2s?

please answer about my question.

 

**description**

Kernel Version : L3.14.28

Application : QT

Labels (1)
0 Kudos
Reply
1 Solution
1,735 Views
igorpadykov
NXP Employee
NXP Employee

Hi jongju

seems custom driver should be designed for such use case, please use

description of hdmi audio driver in sect.16.2.5 Audio attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,736 Views
igorpadykov
NXP Employee
NXP Employee

Hi jongju

seems custom driver should be designed for such use case, please use

description of hdmi audio driver in sect.16.2.5 Audio attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,735 Views
jongjupark
Contributor I

Thank you. Your answer ^^

I need to create the necessary driver.

0 Kudos
Reply