Hello Josu,
Many computer manufacturers do not clearly mark USB port versions. Use the Device Manager to determine if your computer has USB 1.1, 2.0, or 3.0 ports:
- Open the Device Manager.
- In the "Device Manager" window, click the + (plus sign) next to Universal Serial Bus controllers. You will see a list of the USB ports installed on your computer.
- If your USB port name contains "Universal Host", your port is version 1.1.
- If the port name contains both "Universal Host" and "Enhanced Host", your port is version 2.0.
- If the port name contains "USB 3.0", your port is version 3.0.