Hi NXP team,
I need some help getting playback audio port OUT-RL, OUT-RR, SW or C on IMX-AUD-IO using AUDIO SLOT 1. I'm using i.MX Android automative-13.0.0_2.3.0 release to build image.
I am able to hear audio via FR and FL but I'm struggling in enabling the other ports on the IMX-AUD-IO board.
Any help is truly appreciated,
Giang
Solved! Go to Solution.
Hello,
Android Automotive release doesn't support multi-channel audio from Android Apps. Only "tinyplay" can work on FR and FL outputs.
To use multichannel audio, the hardware and driver should support multichannel audio, it is up to customer to implement it since our release uses stereo output.
This link could be useful as reference:
Automotive Audio | Android Open Source Project
Configure audio policies | Android Open Source Project
Best regards.
Hello,
Android Automotive release doesn't support multi-channel audio from Android Apps. Only "tinyplay" can work on FR and FL outputs.
To use multichannel audio, the hardware and driver should support multichannel audio, it is up to customer to implement it since our release uses stereo output.
This link could be useful as reference:
Automotive Audio | Android Open Source Project
Configure audio policies | Android Open Source Project
Best regards.