How can I debug the M4 core on a imx6 using JTAG?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I debug the M4 core on a imx6 using JTAG?

1,139 Views
aaronpadilla
Contributor II

I am trying to debug the M4 processor, according to  below discussion, I should be capable to use the j-link debugger using a script file but I dont understand is this method is for the IAR or the ds5, are there a guide for debug the M4 using the JTAG interface?

How to configure Real View ICE and RealView debugger to work with i.MX6 SoloX

I am using Rowley Crossworks, an eclipse based IDE with ARM gcc, could I use it to debug the M4 with a j-link debugger?

Thanks in advance

Labels (1)
0 Kudos
1 Reply

680 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aaron

link is for DS5 debugger, for jlink one can look at

I.MX6SX SoloX Debugging

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos