I've installed yocto and all required dependencies on an Ubuntu 14.04 LTS build.
I walked through the setup instructions for the fsl-community-bsp.
imx6dqscm-1gb-qwks source fsl-setup-release.sh -b build-fsl-arm-yocto
bitbake core-image-minimal
I don't want / need the gui based distro's that are offered on the Freescale bsp for this board. Is there some way to get a core-image-minimal built for this board. Every time I set the distro I want, it still revers to the x11 / qt5 / wayland distro's anyways.
Is there an easy way to add just the layer I need? I believe this layer would work:
GitHub - juan-gutierrez/meta-nxp-imx-scm: SCM Yocto Meta layer
But how do I add that layer to either the FSL-Community source or the Freescale provided source?
Is there no official support for the SCM line? There's a disturbing lack of documentation online about this chipset.
Thanks!
Hello Matthew Bach,
Have you tried following the document bellow? It covers how to build for this machine and you should be able to bake the core-image-minimal with it.
https://community.nxp.com/docs/DOC-333955
The distro configuration would be ignored when baking the core-image-minimal image as it does not have a GUI. If you have already created a build directory with certain local.conf configurations you may initialize the environment using:
$ source setup-environment <Existing_BUILD_DIR>
This way your build directory configuration won’t be overwritten.
I hope this information helps!
Regards,
It's failing to find this manifest:
Get https://gerrit.googlesource.com/git-repo/clone.bundle
Get https://gerrit.googlesource.com/git-repo
Get git://git.freescale.com/imx/fsl-arm-yocto-bsp.git
fatal: Couldn't find remote ref refs/heads/scm-imx-4.1-krogoth
fatal: Couldn't find remote ref refs/heads/scm-imx-4.1-krogoth
fatal: cannot obtain manifest git://git.freescale.com/imx/fsl-arm-yocto-bsp.git
Hello Matthew Bach,
Were you able to get the git to work? Sometimes they fail but it's usually temporary.
I was able to run it with:
$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1-krogoth -m scm-imx-4.1.15-2.0.0.xml
$ repo sync
Regards,
Yes, it is working for me now, thanks.
I believe so, but I can't confirm it completely yet. The document looks
identical to the pdf included with the imx6dqscm-1gb-qwks board
documentation, but the link to the repo could be slightly different. I'll
give this a shot and get back to you. If it is the same one, then it does
not allow you to compile for core-image-minimal.