How can I change the target of my U-boot from SD Card to NAND?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I change the target of my U-boot from SD Card to NAND?

3,398 次查看
p01049199539
Contributor II

Hello, everybody.

I want to change u-boot's Config from SD Card to NAND.

However, an error will occur even if you proceed as shown in the manual and the following link.

* manual name = i.MX_Yocto_Project_User's_Guide_Linux.pdf (attached)

* Follow Link = http://cache.freescale.com/files/training/doc/ftf/2014/FTF-SDS-F0106.pdf

The error content is as follows:

---------------------------------------------------------------------------------------------------------------------------------------------------------------

test@test-VirtualBox:~/fsl-release-bsp$ MACHINE=imx6qsabresd source setup-environment test_pms/

test@test-VirtualBox:~/fsl-release-bsp/test_pms$ bitbake -c deploy u-boot-imx
Loading cache: 100% |##########################################################################################################################| ETA: 00:00:00
Loaded 2211 entries from dependency cache.
ERROR: Nothing PROVIDES 'u-boot-imx'
ERROR: u-boot-imx was skipped: You cannot use UBOOT_MACHINE and UBOOT_CONFIG at the same time.
ERROR: u-boot-imx was skipped: UBOOT_CONFIG nand is not supported
ERROR: u-boot-imx was skipped: UBOOT_CONFIG nand is not supported

Summary: There was 1 ERROR message shown, returning a non-zero exit code.

---------------------------------------------------------------------------------------------------------------------------------------------------------------

Do I need to do something else before I follow the manual?

The manual only says that UBOOT_CONFIG should be modified as follows: UBOOT_CONFIG = "nand"

I confirmed that my kernel and dtb were working successfully (made according to the manual).
But only u-boot can't change to NAND...

The version of u-boot I use is confirmed to be v2014.01-r0.

(The version of u-boot that is currently created.)

We need your help!

0 项奖励
回复
2 回复数

3,217 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复

3,217 次查看
p01049199539
Contributor II

Dear Joan Xie

Thank you for your reply.
Also, thank you for providing me with the necessary information in the future.

However, when UBOOT_CONFIG = "nand" was applied, the reason for the error could not be determined.
It also failed to determine how to resolve the error.

When I follow your link, it appears that UBOOT_MACHINE and UBOOT_CONFIG are not available at the same time.

Does UBOOT_CONFIG = "nand" require a different procedure?

I need your help.

0 项奖励
回复