I'm using imx8mq evk.
How can I change the mode of vpu of imx8mq to overdrive mode? I know it's not recommended, but I want to change the mode of operation of vpu for the test.
If I print out the gpu clock, I get 800 MHz. Isn't the overdrive mode 1000 MHz?
When I read the imx gpu document, it says that if I enter the command as follows, it will change to overdrive mode:
sudo echo "overdrive"> /sys/bus/platform/drivers/galcore/gpu_govern.
However, my file system does not have "gpu_govern". Is there a way to change it?
refer to the imx8mq reference manual,
i.mx8mq supports override mode of VPU as default