How can I boot from external SD card of MCIMX93EVK (I.mx93 evk)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I boot from external SD card of MCIMX93EVK (I.mx93 evk)?

Jump to solution
2,560 Views
gyyang
Contributor I

Hello,

I am trying to boot from external SD card of I.mx93 EVK.

I made a SD card according to the i.mx linux user manual 4.3.2.

      sudo dd if=imx-image-multimedia-imx93evk.wic of=/dev/mmcblk0 bs=1M && sync

I changed the boot mode switch (SW1301) to 0010 for SD card boot. And installed sd card and turn on.

But nothing happened. I could see no debug message from debug port.

Is there anyone who can download image to external SD card and boot correctly?

Thanks.

 

0 Kudos
Reply
1 Solution
2,522 Views
Harvey021
NXP TechSupport
NXP TechSupport

That is correct. 

 

Regards

Harvey

View solution in original post

0 Kudos
Reply
4 Replies
2,535 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi 

The BMODE should be as SW1301-1: 0, SW1301-2: 1, SW1301-3: 0, SW1301-4: 0 for SD Card boot instead of 0010.

 

Regards

Harvey

 

0 Kudos
Reply
2,527 Views
gyyang
Contributor I

Thank you for your reply!

I think attached is the right setting for SD card boot, isn't it?

Regards,

 

0 Kudos
Reply
2,523 Views
Harvey021
NXP TechSupport
NXP TechSupport

That is correct. 

 

Regards

Harvey

0 Kudos
Reply
2,448 Views
gyyang
Contributor I

Thanks.

I found that my board has A0 silicon that is not supported by latest release.

0 Kudos
Reply