Hi All
I'm using Android 6.0 to build my image.
And the CPU that I developing is i.MX 6 sabresd DL.
Now I'm trying to design a button that will detect during uboot.
If the button be pressed than will get into recovery mode.
So I need to make an interrupt in uboot.
How to do it?
 
					
				
		
I was just looking at this in the NXP distribution of Android 8. The uboot for mx6sabresd already has support for entering fastboot/recovery mode. They don't use an interrupt, just read the state of the switch at a point during boot time, so it requires the user to press and hold through the time the switch is read, but from what I understand that is normal behaviour.
see mx6sabresd.c\mx6sabresd\freescale\board - uboot-imx - i.MX U-Boot
and look for CONFIG_FSL_FASTBOOT
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi victor
please look on
arm - Handling gpio Interrupts in u-boot - Stack Overflow
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------