How booting Android on imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How booting Android on imx6

3,235 次查看
alexandredel
Contributor I

Hello, sorry for my english, it's not my mother tongue.

I have a sabrelite and i'm trying to put android on it.

I used the linaro image of android : Linaro Releases  but when i put it on a sd card and i plug it in the sabrelite, here is what happened:

## Booting kernel from Legacy Image at 10000000 ...

   Image Name:   Linux-3.2.0+

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3862688 Bytes = 3.7 MiB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 12000000 ...

   Image Name:   Android Ramdisk Image

   Image Type:   ARM Linux RAMDisk Image (gzip compressed)

   Data Size:    196567 Bytes = 192 KiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 11ff0000

   Booting using the fdt blob at 0x11ff0000

   Loading Kernel Image ... OK

OK

   Using Device Tree in place at 11ff0000, end 11ff6b93

Starting kernel ...

<6>Booting Linux on physical CPU 0

<6>Initializing cgroup subsys cpuset

<5>Linux version 3.2.0+ (jenkins-build@ip-10-224-54-183) (gcc version 4.6.3 (Linaro GCC 4.6-2012.03) ) #1 SMP PREEMPT Mon Mar 26 15:12:12 UTC 2012

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

<6>Machine: Freescale i.MX6 Quad (Device Tree), model: Freescale i.MX6 Quad SABRE Lite Board

[    0.000000] Booting Linux on physical CPU 0

[    0.000000] Initializing cgroup subsys cpuset

[    0.000000] Linux version 3.2.0+ (jenkins-build@ip-10-224-54-183) (gcc version 4.6.3 (Linaro GCC 4.6-2012.03) ) #1 SMP PREEMPT Mon Mar 26 15:12:12 UTC 2012

[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d

[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

[    0.000000] Machine: Freescale i.MX6 Quad (Device Tree), model: Freescale i.MX6 Quad SABRE Lite Board

<6>bootconsole [earlycon0] enabled

[    0.000000] bootconsole [earlycon0] enabled

Memory policy: ECC disabled, Data cache writealloc

[    0.000000] Memory policy: ECC disabled, Data cache writealloc

<7>On node 0 totalpages: 229376

<7>free_area_init_node: node 0, pgdat c0803820, node_mem_map c0987000

<7>  Normal zone: 1584 pages used for memmap

<7>  Normal zone: 0 pages reserved

<7>  Normal zone: 178640 pages, LIFO batch:31

<7>  HighMem zone: 720 pages used for memmap

<7>  HighMem zone: 48432 pages, LIFO batch:15

<6>PERCPU: Embedded 8 pages/cpu @c1296000 s10688 r8192 d13888 u32768

[    0.000000] PERCPU: Embedded 8 pages/cpu @c1296000 s10688 r8192 d13888 u32768

<7>pcpu-alloc: s10688 r8192 d13888 u32768 alloc=8*4096

<7>pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 227072

[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 227072

<5>Kernel command line: console=ttymxc0,115200n8 rootwait ro earlyprintk rootdelay=1 fixrtc nocompcache di1_primary tve init=/init androidboot.console=ttymxc0

[    0.000000] Kernel command line: console=ttymxc0,115200n8 rootwait ro earlyprintk rootdelay=1 fixrtc nocompcache di1_primary tve init=/init androidboot.console=ttymxc0

<6>PID hash table entries: 4096 (order: 2, 16384 bytes)

[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)

<6>Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

<6>Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

<6>Memory:[    0.000000] Memory: 896MB 896MB = 896MB total

= 896MB total

<5>Memory: 897324k/897324k available, 151252k reserved, 196608K highmem

[    0.000000] Memory: 897324k/897324k available, 151252k reserved, 196608K highmem

<5>Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xec800000 - 0xf4000000   ( 120 MB)

    lowmem  : 0xc0000000 - 0xec000000   ( 704 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .text : 0xc0008000 - 0xc077027c   (7585 kB)

      .init : 0xc0771000 - 0xc07ba9c0   ( 295 kB)

      .data : 0xc07bc000 - 0xc0805f70   ( 296 kB)

       .bss : 0xc0805f94 - 0xc0986770   (1538 kB)

[    0.000000] Virtual kernel memory layout:

[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)

[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

[    0.000000]     vmalloc : 0xec800000 - 0xf4000000   ( 120 MB)

[    0.000000]     lowmem  : 0xc0000000 - 0xec000000   ( 704 MB)

[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)

[    0.000000]       .text : 0xc0008000 - 0xc077027c   (7585 kB)

[    0.000000]       .init : 0xc0771000 - 0xc07ba9c0   ( 295 kB)

[    0.000000]       .data : 0xc07bc000 - 0xc0805f70   ( 296 kB)

[    0.000000]        .bss : 0xc0805f94 - 0xc0986770   (1538 kB)

<6>Preemptible hierarchical RCU implementation.

[    0.000000] Preemptible hierarchical RCU implementation.

<6>NR_IRQS:432

[    0.000000] NR_IRQS:432

<6>L310 cache controller enabled

[    0.000000] L310 cache controller enabled

<6>l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B

[    0.000000] l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B

<6>sched_clock: 32 bits at 8MHz, resolution 121ns, wraps every 520602ms

[    0.000000] sched_clock: 32 bits at 8MHz, resolution 121ns, wraps every 520602ms

<6>Console: colour dummy device 80x30

[    0.000000] Console: colour dummy device 80x30

<3>ram_console: buffer   (null), invalid size 0, datasize 4294967284

[    0.000000] ram_console: buffer   (null), invalid size 0, datasize 4294967284

<6>Calibrating delay loop... [    0.024213] Calibrating delay loop... <c>1581.05 BogoMIPS (lpj=7905280)

1581.05 BogoMIPS (lpj=7905280)

<6>pid_max: default: 32768 minimum: 301

[    0.121267] pid_max: default: 32768 minimum: 301

<6>Mount-cache hash table entries: 512

[    0.129883] Mount-cache hash table entries: 512

<6>CPU: Testing write buffer coherency: [    0.143930] CPU: Testing write buffer coherency: ok

ok

<6>ftrace: allocating 20020 entries in 59 pages

[    0.153618] ftrace: allocating 20020 entries in 59 pages

<6>CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

[    0.192282] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

<6>Calibrating local timer... [    0.200779] Calibrating local timer... 396.19MHz.

396.19MHz.

<6>hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

[    0.267415] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

CPU1: Booted secondary processor

<6>CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

CPU2: Booted secondary processor

<6>CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

CPU3: Booted secondary processor

<6>CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

<6>Brought up 4 CPUs

[    0.373827] CPU1: Booted secondary processor

[    0.415037] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

[    0.453856] CPU2: Booted secondary processor

[    0.495074] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

[    0.533891] CPU3: Booted secondary processor

[    0.575112] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

[    0.577094] Brought up 4 CPUs

<6>SMP: Total of 4 processors activated (6324.22 BogoMIPS).

[    0.615823] SMP: Total of 4 processors activated (6324.22 BogoMIPS).

<6>devtmpfs: initialized

[    0.625689] devtmpfs: initialized

<6>print_constraints: dummy:

[    0.638646] print_constraints: dummy:

<6>NET: Registered protocol family 16

[    0.646364] NET: Registered protocol family 16

<7>gpiochip_find_base: found new base at 224

<7>gpiochip_find_base: found new base at 192

<7>gpiochip_find_base: found new base at 160

<7>gpiochip_find_base: found new base at 128

<7>gpiochip_find_base: found new base at 96

<7>gpiochip_find_base: found new base at 64

<7>gpiochip_find_base: found new base at 32

<4>audmux_v2 21d8000.audmux: audmux_v2_probe: cannot get clock: 0

[    0.705089] audmux_v2 21d8000.audmux: audmux_v2_probe: cannot get clock: 0

<6>cpaddr = ec880000 suspend_iram_base=ec826000

[    0.723355] cpaddr = ec880000 suspend_iram_base=ec826000

<6>No ATAGs?[    0.729874] No ATAGs?<6>hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

[    0.738989] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

<6>hw-breakpoint: maximum watchpoint size is 4 bytes.

[    0.752183] hw-breakpoint: maximum watchpoint size is 4 bytes.

<6>bio: create slab <bio-0> at 0

[    0.789841] bio: create slab <bio-0> at 0

<5>SCSI subsystem initialized

[    0.799597] SCSI subsystem initialized

<7>libata version 3.00 loaded.

<6>usbcore: registered new interface driver usbfs

[    0.812355] usbcore: registered new interface driver usbfs

<6>usbcore: registered new interface driver hub

[    0.822626] usbcore: registered new interface driver hub

<6>usbcore: registered new device driver usb

[    0.832350] usbcore: registered new device driver usb

<6>imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

[    0.871857] imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

<6>imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

[    0.901866] imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

<6>Advanced Linux Sound Architecture Driver Version 1.0.24.

[    0.915767] Advanced Linux Sound Architecture Driver Version 1.0.24.

<6>Switching to clocksource mxc_timer1

[    0.927175] Switching to clocksource mxc_timer1

<6>NET: Registered protocol family 2

[    0.982644] NET: Registered protocol family 2

<6>IP route cache hash table entries: 32768 (order: 5, 131072 bytes)

[    0.993483] IP route cache hash table entries: 32768 (order: 5, 131072 bytes)

<6>TCP established hash table entries: 131072 (order: 8, 1048576 bytes)

[    1.007805] TCP established hash table entries: 131072 (order: 8, 1048576 bytes)

<6>TCP bind hash table entries: 65536 (order: 7, 786432 bytes)

[    1.022839] TCP bind hash table entries: 65536 (order: 7, 786432 bytes)

<6>TCP: Hash tables configured (established 131072 bind 65536)

[    1.036247] TCP: Hash tables configured (established 131072 bind 65536)

<6>TCP reno registered

[    1.045081] TCP reno registered

<6>UDP hash table entries: 512 (order: 2, 16384 bytes)

[    1.053207] UDP hash table entries: 512 (order: 2, 16384 bytes)

<6>UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

[    1.064588] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

<6>NET: Registered protocol family 1

[    1.074731] NET: Registered protocol family 1

<6>RPC: Registered named UNIX socket transport module.

[    1.084603] RPC: Registered named UNIX socket transport module.

<6>RPC: Registered udp transport module.

[    1.094330] RPC: Registered udp transport module.

<6>RPC: Registered tcp transport module.

[    1.102820] RPC: Registered tcp transport module.

<6>RPC: Registered tcp NFSv4.1 backchannel transport module.

[    1.113045] RPC: Registered tcp NFSv4.1 backchannel transport module.

<6>Trying to unpack rootfs image as initramfs...

[    1.124219] Trying to unpack rootfs image as initramfs...

<6>Freeing initrd memory: 192K

[    1.146718] Freeing initrd memory: 192K

<6>i.MXC CPU frequency driver

[    1.154043] i.MXC CPU frequency driver

<6>audit: initializing netlink socket (disabled)

[    1.163002] audit: initializing netlink socket (disabled)

<5>type=2000 audit(1.080:1): initialized

[    1.172229] type=2000 audit(1.080:1): initialized

highmem bounce pool size: 64 pages

[    1.196554] highmem bounce pool size: 64 pages

<6>ashmem: initialized

[    1.203711] ashmem: initialized

<6>Btrfs loaded

[    1.211343] Btrfs loaded

<6>msgmni has been set to 1368

[    1.216810] msgmni has been set to 1368

<6>Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252)

[    1.228313] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 252)

<6>io scheduler noop registered

[    1.238723] io scheduler noop registered

<6>io scheduler deadline registered

[    1.245987] io scheduler deadline registered

<6>io scheduler cfq registered (default)

[    1.254129] io scheduler cfq registered (default)

<6>mxc_sdc_fb 0.fb: register mxc display driver ldb

[    1.266959] mxc_sdc_fb 0.fb: register mxc display driver ldb

<3>_regulator_get: get() with no identifier

[    1.276703] _regulator_get: get() with no identifier

<4>imx-ipuv3 imx-ipuv3.1: Channel already disabled 9

<4>imx-ipuv3 imx-ipuv3.1: Channel already uninitialized 9

<6>imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

[    1.286616] imx-ipuv3 imx-ipuv3.1: Channel already disabled 9

[    1.291772] imx-ipuv3 imx-ipuv3.1: Channel already uninitialized 9

[    1.319019] imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

<6>Console: switching to colour frame buffer device 128x48

[    1.370801] Console: switching to colour frame buffer device 128x48

<4>imx-ipuv3 imx-ipuv3.1: Channel already disabled 10

<4>imx-ipuv3 imx-ipuv3.1: Channel already uninitialized 10

[    1.392232] imx-ipuv3 imx-ipuv3.1: Channel already disabled 10

[    1.397507] imx-ipuv3 imx-ipuv3.1: Channel already uninitialized 10

<6>mxc_sdc_fb 1.fb: register mxc display driver hdmi

[    1.418108] mxc_sdc_fb 1.fb: register mxc display driver hdmi

<6>mxc_hdmi mxc_hdmi: Detected HDMI controller 0x13:0xa:0xa0:0xc1

[    1.429845] mxc_hdmi mxc_hdmi: Detected HDMI controller 0x13:0xa:0xa0:0xc1

<4>imx-ipuv3 imx-ipuv3.0: Channel already disabled 9

<4>imx-ipuv3 imx-ipuv3.0: Channel already uninitialized 9

[    1.441649] imx-ipuv3 imx-ipuv3.0: Channel already disabled 9

[    1.446802] imx-ipuv3 imx-ipuv3.0: Channel already uninitialized 9

<4>imx-ipuv3 imx-ipuv3.0: Channel already disabled 10

<4>imx-ipuv3 imx-ipuv3.0: Channel already uninitialized 10

[    1.479399] imx-ipuv3 imx-ipuv3.0: Channel already disabled 10

[    1.484641] imx-ipuv3 imx-ipuv3.0: Channel already uninitialized 10

<6>imx-sdma 20ec000.sdma: loaded firmware 1.1

im   1.505172] imx-sdma 20ec000.sdma: loaded firmware 1<6.>1

x-sdma 20ec000.sdma: initialized

[    1.51380<36>] Seirmxia-sl:dm aIM 2X 0decr0iv00er.

ar: <i6>ni21tiea8l00i0ze.ud                          sd

t: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX

[    1.518779] Serial: IMX driver

[    1.525914] 21e8000.uart: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX

<6>imx-ocotp 21bc000.ocotp: initialized

[    1.737889] imx-ocotp 21bc000.ocotp: initialized

<6>brd: module loaded

[    1.759595] brd: module loaded

<6>loop: module loaded

[    1.772777] loop: module loaded

<6>No sata disk, enter into PDDQ mode.

[    2.383903] No sata disk, enter into PDDQ mode.

<4>m25p80 spi32766.0: found sst25vf016b, expected m25p32

[    2.397293] m25p80 spi32766.0: found sst25vf016b, expected m25p32

<6>m25p80 spi32766.0: sst25vf016b (2048 Kbytes)

[    2.407906] m25p80 spi32766.0: sst25vf016b (2048 Kbytes)

<6>spi_imx 2008000.ecspi: probed

[    2.417477] spi_imx 2008000.ecspi: probed

<6>FEC Ethernet Driver

[    2.425176] FEC Ethernet Driver

<6>fec_enet_mii_bus: probed

[    2.448304] fec_enet_mii_bus: probed

<6>usbcore: registered new interface driver asix

[    2.457828] usbcore: registered new interface driver asix

<6>usbcore: registered new interface driver cdc_ether

[    2.468362] usbcore: registered new interface driver cdc_ether

<6>usbcore: registered new interface driver smsc95xx

[    2.479330] usbcore: registered new interface driver smsc95xx

<6>usbcore: registered new interface driver net1080

[    2.490033] usbcore: registered new interface driver net1080

<6>usbcore: registered new interface driver cdc_subset

[    2.500920] usbcore: registered new interface driver cdc_subset

<6>usbcore: registered new interface driver zaurus

[    2.511699] usbcore: registered new interface driver zaurus

<6>cdc_ncm: 04-Aug-2011

[    2.519622] cdc_ncm: 04-Aug-2011

<6>usbcore: registered new interface driver cdc_ncm

[    2.527795] usbcore: registered new interface driver cdc_ncm

<6>ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

[    2.539631] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

<7>ehci_hcd: block sizes: qh 64 qtd 96 itd 160 sitd 96

<6>mxc-ehci ehci-mxc.0: initializing i.MX USB Controller

[    2.556396] mxc-ehci ehci-mxc.0: initializing i.MX USB Controller

<6>mxc-ehci ehci-mxc.0: Freescale On-Chip EHCI Host Controller

[    2.597475] mxc-ehci ehci-mxc.0: Freescale On-Chip EHCI Host Controller

<6>mxc-ehci ehci-mxc.0: new USB bus registered, assigned bus number 1

[    2.610824] mxc-ehci ehci-mxc.0: new USB bus registered, assigned bus number 1

<7>mxc-ehci ehci-mxc.0: reset hcs_params 0x10011 dbg=0 ind cc=0 pcc=0 ordered ports=1

<7>mxc-ehci ehci-mxc.0: reset hcc_params 0006 thresh 0 uframes 256/512/1024 park

<7>mxc-ehci ehci-mxc.0: park 0

<7>mxc-ehci ehci-mxc.0: reset command 0080002 (park)=0 ithresh=8 period=1024 Reset HALT

<7>mxc-ehci ehci-mxc.0: ...powerdown ports...

<6>mxc-ehci ehci-mxc.0: irq 75, io mem 0x02184000

[    2.676370] mxc-ehci ehci-mxc.0: irq 75, io mem 0x02184000

<7>mxc-ehci ehci-mxc.0: init command 0010005 (park)=0 ithresh=1 period=512 RUN

<6>mxc-ehci ehci-mxc.0: USB 2.0 started, EHCI 1.00

[    2.706447] mxc-ehci ehci-mxc.0: USB 2.0 started, EHCI 1.00

<7>usb usb1: default language 0x0409

<7>usb usb1: udev 1, busnum 1, minor = 0

<6>usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

[    2.725048] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

<6>usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

[    2.738161] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

<6>usb usb1: Product: Freescale On-Chip EHCI Host Controller

[< 6 > us 2b. u75sb0191: 5]Ma unsufb acutsbur1:er P:r Lodinuuctx : 3.Fr2e.0es+ cealhce i_Onh-cdCh

ip< 6>EHuCsbI  uHsosb1t : CSonetrriaolllNuermb

: ehci-mxc.0

[    2.7<759>u6s33b ] uussb1b: u usbs1b:_ prMaobneuf_dacetvuicreer

: <7L>inuusbx  3us.2b.10: +c eonhcfii_guhrcdat

n[   #1   2ch.7o6s5en2 02fr] oums 1b  uchsbo1i:ce

r<i7>aulNsbum buesbr1: : ehacddi-inmgxc 1.0-0     Se

1.0 (config #1, interface 0)

<7>hub 1-0:1.0: usb_probe_interface

<7>hub 1-0:1.0: usb_probe_interface - got id

<6>hub 1-0:1.0: USB hub found

[    2.797478] hub 1-0:1.0: USB hub found

<6>hub 1-0:1.0: 1 port detected

[    2.804223] hub 1-0:1.0: 1 port detected

<7>hub 1-0:1.0: standalone hub

<7>hub 1-0:1.0: individual port power switching

<7>hub 1-0:1.0: individual port over-current protection

<7>hub 1-0:1.0: Single TT

<7>hub 1-0:1.0: TT requires at most 8 FS bit times (666 ns)

<7>hub 1-0:1.0: power on to power good time: 20ms

<7>hub 1-0:1.0: local power source is good

<7>hub 1-0:1.0: enabling power on all ports

<6>mxc-ehci ehci-mxc.1: initializing i.MX USB Controller

[    2.846019] mxc-ehci ehci-mxc.1: initializing i.MX USB Controller

<7>hub 1-0:1.0: state 7 ports 1 chg 0000 evt 0000

<6>mxc-ehci ehci-mxc.1: Freescale On-Chip EHCI Host Controller

[    <62.>m94xc74-e89h]c i mexchc-eih-cmxic e.1hc:i n-mexwc U.S1:B  Fbrues erscegalies teOrn-edCh,i pas sEHigCIn eHd obstus C onnumtbroerll e2r

7>mxc-ehci ehci-mxc.1: reset hcs_params 0x10011 dbg=0 ind cc=0 pcc=0 ordered ports=1

[< 7 >m  x2c-.9eh6c02i 11e]h cim-xcmx-ech.c1:i  erhesciet- mxhcc.c_1:p arneamws U 0SB00 b6u ts hrreegshis 0te rufedra,m aesss 2ig5n6/ed51 2bu/1s 02nu4m pbearrk 2

<7>mxc-ehci ehci-mxc.1: park 0

<7>mxc-ehci ehci-mxc.1: reset command 0080b02  park=3 ithresh=8 period=1024 Reset HALT

<7>mxc-ehci ehci-mxc.1: ...powerdown ports...

<6>mxc-ehci ehci-mxc.1: irq 72, io mem 0x02184200

[    3.026389] mxc-ehci ehci-mxc.1: irq 72, io mem 0x02184200

<7>mxc-ehci ehci-mxc.1: init command 0010005 (park)=0 ithresh=1 period=512 RUN

<6>mxc-ehci ehci-mxc.1: USB 2.0 started, EHCI 1.00

[    3.056451] mxc-ehci ehci-mxc.1: USB 2.0 started, EHCI 1.00

<7>usb usb2: default language 0x0409

<7>usb usb2: udev 1, busnum 2, minor = 128

<6>usb usb2: New USB device found, idVendor=1d6b, idProduct=0002

[    3.075205] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002

<6>usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1

[    3.088306] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1

<6>usb usb2: Product: Freescale On-Chip EHCI Host Controller

[    3.101053] usb usb2: Product: Freescale On-Chip EHCI Host Controller

<6>usb usb2: Manufacturer: Linux 3.2.0+ ehci_hcd

[    3.111971] usb usb2: Manufacturer: Linux 3.2.0+ ehci_hcd

<6>usb usb2: SerialNumber: ehci-mxc.1

[    3.120885] usb usb2: SerialNumber: ehci-mxc.1

<7>usb usb2: usb_probe_device

<7>usb usb2: configuration #1 chosen from 1 choice

<7>usb usb2: adding 2-0:1.0 (config #1, interface 0)

<7>hub 2-0:1.0: usb_probe_interface

<7>hub 2-0:1.0: usb_probe_interface - got id

<6>hub 2-0:1.0: USB hub found

[    3.148438] hub 2-0:1.0: USB hub found

<6>hub 2-0:1.0: 1 port detected

[    3.155197] hub 2-0:1.0: 1 port detected

<7>hub 2-0:1.0: standalone hub

<7>hub 2-0:1.0: individual port power switching

<7>hub 2-0:1.0: individual port over-current protection

<7>hub 2-0:1.0: Single TT

<7>hub 2-0:1.0: TT requires at most 8 FS bit times (666 ns)

<7>hub 2-0:1.0: power on to power good time: 20ms

<7>hub 2-0:1.0: local power source is good

<7>hub 2-0:1.0: enabling power on all ports

<6>usbcore: registered new interface driver cdc_wdm

[    3.197053] usbcore: registered new interface driver cdc_wdm

<6>Initializing USB Mass Storage driver...

[    3.206675] Initializing USB Mass Storage driver...

<6>usbcore: registered new interface driver usb-storage

[    3.216956] usbcore: registered new interface driver usb-storage

<6>USB Mass Storage support registered.

[    3.226669] USB Mass Storage support registered.

<6>usbcore: registered new interface driver libusual

[    3.236378] usbcore: registered new interface driver libusual

<6>usbcore: registered new interface driver usbtest

[    3.247118] usbcore: registered new interface driver usbtest

<3>egalax_ts 2-0004: egalax_ts: failed to read firmware version

[    3.259045] egalax_ts 2-0004: egalax_ts: failed to read firmware version

<4>egalax_ts: probe of 2-0004 failed with error -5

[    3.270419] egalax_ts: probe of 2-0004 failed with error -5

<6>using rtc device, 20cc000.snvs, for alarms[    3.282836] using rtc device, 20cc000.snvs, for alarms<7>mxc-ehci ehci-mxc.1: GetStatus port:1 status 10001803 8  ACK POWER sig=j CSC CONNECT

<7>hub 2-0:1.0: port 1: status 0101 change 0001

<6>snvs_rtc 20cc000.snvs: rtc core: registered 20cc000.snvs as rtc0

[    3.306304] snvs_rtc 20cc000.snvs: rtc core: registered 20cc000.snvs as rtc0

<6>i2c /dev entries driver

[    3.316263] i2c /dev entries driver

<6>Linux video capture interface: v2.00

[    3.324699] Linux video capture interface: v2.00

<6>mxc_v4l2_output v4l2-out.5: V4L2 device registered as video16

[    3.335977] mxc_v4l2_output v4l2-out.5: V4L2 device registered as video16

<6>mxc_v4l2_output v4l2-out.5: V4L2 device registered as video17

[    3.348997] mxc_v4l2_output v4l2-out.5: V4L2 device registered as video17

<6>mxc_v4l2_output v4l2-out.5: V4L2 device registered as video18

[    3.362039] mxc_v4l2_output v4l2-out.5: V4L2 device registered as video18

<6>mxc_v4l2_output v4l2-out.5: V4L2 device registered as video19

[    3.375065] mxc_v4l2_output v4l2-out.5: V4L2 device registered as video19

<6>Driver for 1-wire Dallas network protocol.

[    3.386291] Driver for 1-wire Dallas network protocol.

<7>hub 2-0:1.0: state 7 ports 1 chg 0002 evt 0000

<6>imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

[    3.403557] imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

<7>hub 2-0:1.0: port 1, status 0101, change 0000, 12 Mb/s

<6>device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhat.com

[    3.425024] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-devel@redhat.com

<4>clk_reg_cpufreq: regulator cpu get failed.

[    3.437728] clk_reg_cpufreq: regulator cpu get failed.

<6>cpuidle: using governor ladder

[    3.446402] cpuidle: using governor ladder

<6>cpuidle: using governor menu

[    3.453480] cpuidle: using governor menu

<6>sdhci: Secure Digital Host Controller Interface driver

[    3.463316] sdhci: Secure Digital Host Controller Interface driver

<6>sdhci: Copyright(c) Pierre Ossman

<7>mxc-ehci ehci-mxc.1: port 1 high speed

[< 7 >m  xc3-.4eh72c9i3 e6h] cisd-hmcxci.: 1:Co pGyetrSigtahtt(usc)  poPirte:rr1 e stOsastumas n1

01205 12  ACK POWER sig=se0 LPM PE CONNECT

<6>sdhci-pltfm: SDHCI platform and OF driver helper

[    3.494072] sdhci-pltfm: SDHCI platform and OF driver helper

<7>mxc: set GPIO 32 to high trigger

<4>sdhci-esdhc-imx 2198000.usdhc: vmmc-supply property in node /soc/aips-bus@02100000/usdhc@02198000 references invalid phandle[    3.514655] sdhci-esdhc-imx 2198000.usdhc: vmmc-supply property in node /sd

[    3.529767] mmc0: no vmmc regulator found

<7>Registered led device: mmc0::

<6>mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using DMA

<6>usb 2-1: new high-speed USB device number 2 using mxc-ehci

<7>mxc: set GPIO 198 to high trigger

[ < 4 >s 3dh.c54i-48e6s1dh]c m-imcm0x: 2 1SD9cHC0I0 0.cuonsdtrhocl: lvermm ocn- su2p19pl80y0 0p.rouspedrhcty [ 2i1n 9n80od00e. u/ssodhc/c]a iupss-inbug sD@M02A1

0[ 0 0/ u 3sd.5h5c0@0326919] cu0s00b  2re-1f:er neencw esh iginh-vaspleided p hUSanB dldeev<6i>cem mnc1u:mb nero  2vm musc inrge gumlxcat-eohrc fio

dn

[    <73.>5Re75gi9s00te] resddh lcied- esdedhvic-cie:mx m m21c19c::00

.usdhc: vmmc-sup<6p>lym mcpr1:o peSDrtHCy Ii cn onntodroe ll/seor c/ona ip21s-9cbu0s00@0.u2s10dh00c 00[/21us9cd0hc00@0.u21s9dhc0c]0 0 usreinfegr DenMAc

invalid phandl<e6>                                                                                                                                    es

U[   in i 3ti.5al81i5ze55d

immc1: no <7vm>Rmceg riesgteurlaedto rl edf oudendv

: Heartbeat

[    3.601322] mmc1: SDHCI controller on 219c000.usdhc [219c000.usdhc] usin<g6 >uDsMAbc

ve[ :  r  e3gi.s6t06er0e21d ] neVPwU i intneitrfiaacliez dedri

er usbhid

[<6  >u  s3bh.6id2:66 U60SB]  uHIsbD ccorore:e  rderigivesrt

6d new inte<6r>faloceg gderri: vcerre uatsbehd id25         er

K log 'log_main'

[   <6 >3l.6og32ge24r6: ] cruesbathiedd : 2U5S6KB  HloIDg  c'looreg_ dervienvters'

[    <36.>l6o38gg59e8r]:  cloreggaetred:  c25re6aKt leod g 25'6lKo g_lrogad 'iolo'g

6>ain'<

logger: created 256K log 'log_system'

[    3.646185] logger: created 256K log 'log_events'

3>[ sg  t l53.006053 067-06]0 0alo: gFgeair:le cdr teao tgedet 2 s56uKpp llyo g 'V'lDDogA_':ra -d1io9

                                                                                                     '

[  <6  >3p.ri6n58t_02c6o]ns tloraggienrts:: c 0re-a0t00ead : 25865K0  <lo--g >' l16o0g_0 symsVt aetm' 1

0 mV normal

[ < 3>  sg3t.6l572000502 0] -0s0gt0al5: 00F0ai 0le-d00 t0ao : gFetai sluedpp tlyo  g'VetDD Asu':pp -ly1 9'

l5A'<:3> -sg1t9                                                                                           V

00[ 0   0- 03.0068a:28 4Fa7]il eprd intot_ creonqusetrstai sntuspp: li0e-0s:00 -a:1 98

0< 3><s--gt> l51600000  0m-V 00at0a 1:2 a00so cmV:  nfaorimleald  t                   5

probe CODEC sgtl5000.0-000a: -19

[ < 3 >a 3s.oc6:92 f34ai9]l edsg ttol5 i00ns0 t0an-0ti0a0ate:  cFaairdle sdg ttlo 50ge0t0- sauudppioly:  '-V19DD

A': -19

6>[A  LS  A3 d.7ev0i18ce33 l] isstgt:

50<600>  0 N-0o0 s0aou:n Fdcaiarledds  tfoou rndeq.

lt suppl<6ie>so:pr o-f19i                          ue

[ us  in 3g. a71rm1/05ar4]mv s7g-ctla95

0 0-000a: asoc: failed to probe CODEC sgtl5000.0-000a: -19

[    3.721077] asoc: failed to instantiate card sgtl5000-audio: -19

[    3.725514] ALSA device list:

[    3.73<602>T12C]P   cu bNoic s rouengidcstaerdres d

nin6>dI.                                              fo

ti[a  li  z3in.7g 3X67FR37M ] noetprlionfik leso: cukseit

g arm/armv7-ca9                                          n

[    3.756271] TCP cubic registered

[    3.762709] Initializing XFRM netlink socket

<6>NET: Registered protocol family 10

[    3.870585] NET: Registered protocol family 10

<6>IPv6 over IPv4 tunneling driver

[    3.879352] IPv6 over IPv4 tunneling driver

<6>NET: Registered protocol family 17

[    3.888207] NET: Registered protocol family 17

<6>NET: Registered protocol family 15

[    3.896213] NET: Registered protocol family 15

<5>Registering the dns_resolver key type

[    3.904466] Registering the dns_resolver key type

<6>VFP support v0.3: [    3.911166] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

uplementor 41 architecture 3 part 30 varia<n7>tu 9sb r 2ev- 1:4

dev 2, busnum 2, minor = 129

<6>ThumbEE CPU extension supported.

<6>usb 2-1: New USB device found, idVendor=0424, idProduct=2513

[< 6> u  sb3. 299-21:77 N9e] w ThUSumBb EdEev CicPeU  sextrteinngsis:o n Mfsur=pp0o, rtPreod.du

=[ 0,    Se3.ri99a8lN45um8b] erus=0b

-1: New <7U>SBus dbe v2-i1ce:  fuosub_npd,ro ibdeV_deendviorc=e0

ur<74,>u isbdP r2-od1:u ctco=2nf51ig3

ation #1 chosen from 1 choice

[  <7  >4us.0b 1206-156: ] auddsbin g2- 21:-1 N:e1.w 0 U(SBco dnfeviig ce#1 ,st irintngesrf: acMefr 0=0)

obod<u7>cth=u0b ,2 S-1er:i1a.0l:Nu umbsebr_p=r0                                                         ,

e_interface

<7>hub 2-1:1.0: usb_probe_interface - got id

<5>Registering SWP/SWPB emulation handler

[< 6>  tu r4.n 04of55f9 b9]oo tRe cgionstseolrie neg arSWlyP/cSonWP0

emulation handler                                                  B

[    4.051882] turn off boot console earlycon0

<6>hub 2-1:1.0: USB hub found

<6>hub 2-1:1.0: 3 ports detected

<7>hub 2-1:1.0: standalone hub

<7>hub 2-1:1.0: individual port power switching

<7>hub 2-1:1.0: individual port over-current protection

<7>hub 2-1:1.0: TT per port

<7>hub 2-1:1.0: TT requires at most 8 FS bit times (666 ns)

<7>hub 2-1:1.0: power on to power good time: 100ms

<7>hub 2-1:1.0: local power source is good

<7>hub 2-1:1.0: enabling power on all ports

<6>snvs_rtc 20cc000.snvs: setting system clock to 1970-01-01 00:00:00 UTC (0)

<4>Warning: unable to open an initial console.

<6>Freeing init memory: 292K

<4>init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.

<7>usb 2-1: link qh256-0001/e8a2e4a0 start 1 [1/0 us]

<7>hub 2-1:1.0: state 7 ports 3 chg 0000 evt 0000

<3>init: cannot open '/initlogo.rle'

<6>mmc0: new high speed SDHC card at address 0007

<6>mmcblk0: mmc0:0007 SD4GB 3.67 GiB

<6> mmcblk0: p1 p2 p3 p4 < p5 p6 p7 >

<6>EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)

<7>hub 1-0:1.0: hub_suspend

<7>usb usb1: bus auto-suspend, wakeup 1

<7>mxc-ehci ehci-mxc.0: suspend root hub

<7>hub 2-1:1.0: hub_suspend

<7>usb 2-1: unlink qh256-0001/e8a2e4a0 start 1 [1/0 us]

<7>usb 2-1: usb auto-suspend, wakeup 1

<6>EXT4-fs (mmcblk0p5): recovery complete

<6>EXT4-fs (mmcblk0p5): mounted filesystem with ordered data mode. Opts: (null)

<6>EXT4-fs (mmcblk0p6): recovery complete

<6>EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: (null)

<4>Disabling lock debugging due to kernel taint

<3>init: service 'console' requires console

<3>init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'

<3>init: service 'console' requires console

<7>hub 2-0:1.0: hub_suspend

<7>usb usb2: bus auto-suspend, wakeup 1

<7>mxc-ehci ehci-mxc.1: suspend root hub

<6>warning: `rild' uses 32-bit capabilities (legacy support in use)

<6>request_suspend_state: wakeup (3->0) at 29110575997 (1970-01-02 00:00:09.402363151 UTC)

<6>alarm_release: clear alarm, pending 0

<6>alarm_release: clear alarm, pending 0

<6>request_suspend_state: wakeup (0->0) at 35353204602 (1970-01-02 00:00:15.644991150 UTC)

I don't know what to do, it looks like something is miising, but i don't know what and i don't know how to fix it. However, on the screen, i cn see the boot sreen of android (steel letters of android with a reflect), a friend said that i have to download the sources of android and build them, is it true?

Best Regards

Alexandre

标签 (2)
标记 (4)
0 项奖励
回复
2 回复数

1,804 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Hi Alexandre,

Have you solved you problem now, if not continue discuss here.

Have a nice day.

Best Regards

Dan

0 项奖励
回复

1,804 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Alexandre

I recommend you to download the sources of android and build it yourself. And then download images build yourself to your board.

Which version android BSP are you using?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复