How To Change The Baudrate on MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How To Change The Baudrate on MX6DL

1,120 Views
tony_l_cai
Contributor III

Hi all,

        How to change the baudrate on uboot 2014? Thank you ~

Labels (3)
0 Kudos
Reply
2 Replies

1,008 Views
b36401
NXP Employee
NXP Employee

Do you meen setting custom baudrate for konsole?

It can be set with changing "115200" into the baudrate you need at this point of boot options:

console=ttymxc0,115200

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,008 Views
tony_l_cai
Contributor III

Hi Victor

Where to change the option ? Not in console by boot cmd, I want to change the bootargs in code, how to do it? Thank you~

0 Kudos
Reply