How SDP is implemented in i.MX 8M Mini?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How SDP is implemented in i.MX 8M Mini?

1,201 Views
kanimozhi_t
Contributor V

Hi,

    I recently looked into the CompuLab's IOT-GATE-iMX8 Evaluation Kit. They've not mentioned anything about the Serial Download Protocol support and UUU tool on their page.

    This has raised the following questions in my mind,

  1. Do all i.MX 8MM processors support SDP by default? Or some tweak/additional hardware is required for enabling the SDP on each SoM?
  2. How SDP implemented in i.MX 8M Mini? Are there any resource available?

Thanks in advance.

Labels (1)
0 Kudos
Reply
1 Reply

1,195 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kanimozhi

 

1.  yes it is supported

2.   one can look at sect.6.1.2.4 Serial Downloader, sect.6.1.8 Serial Downloader

i.MX 8M Mini Applications Processor Reference Manual

 

Best regards
igor