How IMX8M drives DDR4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How IMX8M drives DDR4

897 Views
haochengdong
Contributor II

Can IMX8M support 2 pieces of 1GbX16 DDR4? Only DRAM_nCS0 is used, and DRAM_nCS1 is left floating. If T PCB routing topology is used, whether 65Ω resistor must be added to VTT on the address and control line. Please give a reference design. Thanks.Is there a corresponding BSP?

0 Kudos
Reply
1 Reply

842 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Haochengdong Haochengdong,

The Reference Design available is the i.MX8MQ EVK (for which Design Files are provided on the NXP website). The recommendations for DDR4 design with the i.MX8MQ can be found on the i.MX8QM Hardware Design Guide (link below, please note that you may need to login to download this document.

https://www.nxp.com/webapp/Download?colCode=IMX8MDQLQHDG

There is also an Application Note that may be useful (AN5097, link below, you may need to login to download this document) that covers hardware and layout considerations for DDR4 designs albeit not for i.MX8QM specifically.

https://www.nxp.com/webapp/Download?colCode=AN5097

I hope this helps!

Regards,

0 Kudos
Reply