Hi there,
In Imx6UL, to disable JTAG, which command I have to use?
Also, as per Application Note AN12419, SJC_DISABLE need to be blown with 1 and JTAG_SMODE[1:0] need to be 11.
Can you particularly guide for command to blow above bits?
Is the SJEC_RESP can be alternate method to above method?
Thank you in advance!
Kavita
Thank you for contacting NXP support!
You have to program the SJC_DISABLE and JTAG_SMODE.
JTAG_SMODE : JTAG Security Mode. Controls the security mode of the JTAG debug interface
Set JTAG security mode
00 - JTAG enable mode
01 - Secure JTAG mode
11 - No debug mode
SJC_DISABLE: Disable/Enable the Secure JTAG Controller module. This fuse is used to create the highest JTAG security level, where JTAG is totally blocked.
0 - Secure JTAG Controller is enabled
1 - Secure JTAG Controller is disabled
you can learn how to program and read the fuses following the link: