Hibernation/resume on IMX6Q board for android.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hibernation/resume on IMX6Q board for android.

2,307件の閲覧回数
johnturnur
Contributor III

Hello,

Has anyone tried to implement hibernation/resume for android on IMX 6Q-SABRESD board. I am able to hibernate it and stored the image on memory, and resumes from image. At the end it successfully restored from hibernate image but command prompt does not display >>root@android. Also screen does not display home screen of android and remains black.

Can anyone Help in this direction?

Regards,

John

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

1,457件の閲覧回数
sudhirdumbhare
Contributor I

Hi John,

Am trying to implement hibernation on IMX6 .

After "PM: Saving image data pages (100869 pages) ...           56%"

this message reboot the device. It is showing not compelete 100%.

Can you give me some direction or help is appreciable.

Regards,

Sudhir

0 件の賞賛
返信

1,457件の閲覧回数
sudhirdumbhare
Contributor I

Hi,

Now am able to create hibernation image & save data pages 100%.

But at Resume, when it trying to load image, return error from

unpack_orig_pfns() function with error value -14.

Any help or direction will help to resolve this thing.

Regards,

Sudhir

0 件の賞賛
返信

1,457件の閲覧回数
johnjohntobias
Contributor II

Hello Guys,

I would like to know if you made progress on the hibernation support and able to fix the crashing?.

Regards,

John

1,457件の閲覧回数
ivanyu
Contributor I

Hi John Turnur:

     About the hibernate for Imx6 board of android platform, I also had implemented it but it will cause kernel panic after create image. Do you have any suggestion or referece codes or resources help me to accomplish your porting currently.Thanks. My email is fantasypro@ms15.url.com.tw

                                                                                                 IVAN

0 件の賞賛
返信

1,457件の閲覧回数
xiongjunhe
Contributor II

Hi ivan yu:

     Have you make it? I want to the hibernation on imx6 linux/Android too.

0 件の賞賛
返信

1,457件の閲覧回数
maximsyrchin
Contributor I

Hello,

Did you solve problem ?
Could you give some glue ? As I can see there is no hibernation for arm platform at all - which kernel did you use ?

Thanks,
Maxim

0 件の賞賛
返信