Hibernate/Resume failure with galcore (gpu-viv) driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hibernate/Resume failure with galcore (gpu-viv) driver

2,929 次查看
ripplejr
Contributor II

I'm working with an i.MX8QXP processor and am having inconsistent crashing during resume from hibernation (suspend to disk). I've narrowed it down to the galcore module causing the issue since it the crash happens only when the galcore module (gpu-viv driver) is loaded. The system will save the image fine but during resume it will fail to decompress the image in every 1 in 4 resumes. The only consistent work fixes that I've found are either using the resume=nocompress option so lzo copmression is never used (causes a large slow down with saving or reading the image) or by setting acpi=off in the kernel options.

This problem has shown up on both the 5.4 and 5.10 kernels.

This problem looks similar to this issue but the patch provided is for a different system.

https://community.nxp.com/t5/i-MX-Processors/GPU-hang-after-multiple-suspend-resume-cycles/m-p/96209...

 

Steps to reproduce:

1. echo reboot > /sys/power/disk; pm-hibernate

 

Error Log during boot:

[ 1.809743] PM: hibernation: resume from hibernation
[ 1.815829] Freezing user space processes ... (elapsed 0.000 seconds) done.
[ 1.822933] OOM killer disabled.
[ 1.826197] Freezing remaining freezable tasks ...
[ 1.828292] mmc1: SDHCI controller on 5b020000.mmc [5b020000.mmc] using ADMA
[ 1.903968] (elapsed 0.077 seconds) done.
[ 1.951290] PM: Using 3 thread(s) for decompression
[ 1.956288] PM: Loading and decompressing image data (201761 pages)...
[ 1.963110] hibernate: Hibernated on CPU 0 [mpidr:0x0]
[ 2.103104] PM: Image loading progress: 0%
[ 2.799921] imx6q-pcie 5f010000.pcie: Phy link never came up
[ 2.805756] imx6q-pcie 5f010000.pcie: failed to initialize host
[ 2.811730] imx6q-pcie 5f010000.pcie: unable to add pcie port.
[ 3.033214] PM: Image loading progress: 10%
[ 3.518651] PM: Image loading progress: 20%
[ 3.764275] PM: Image loading progress: 30%
[ 4.013727] PM: Image loading progress: 40%
[ 4.027386] PM: LZO decompression failed
[ 4.031422] PM: hibernation: Read 807044 kbytes in 2.06 seconds (391.76 MB/s)
[ 4.046593] PM: hibernation: Failed to load image, recovering.
[ 4.319290] OOM killer enabled.
[ 4.322518] Restarting tasks ... done.
[ 4.327082] PM: hibernation: resume failed (-4)

0 项奖励
回复
6 回复数

2,916 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello ripplejr,

Please do you use the latest BSP? Can you please state the detailed duplicated steps?

Can you please provide the detailed failure log for the failure? It hangs before suspend or after resume?

Do this happens only for Android?

 

Regards

 

0 项奖励
回复

2,912 次查看
ripplejr
Contributor II

I'm currently using the 5.10.72 release.

Steps to reproduce.

1) echo disk > /sys/power/state

This is the only step to do, if hibernation is enabled in the kernel config and there is a swap space for the image then running the above command will cause the issue. This only happens in 1 in 4 hibernations and only on the resume. When the kernel is loading the image during resume, LZO decompression fails. This is not on Android but a custom Linux build.

0 项奖励
回复

2,908 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

ok, it looks like and issue, don't enable at the moment the kernel hypervisor, will check with the developers.

 

Thanks for the catch!

0 项奖励
回复

2,900 次查看
ripplejr
Contributor II

I tried turning off the hypervisor but it doesn't seem to do anything. The LZO compression error still shows up.

0 项奖励
回复

2,890 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

The i.MX8QXP do not support hypervisor, it support jailhouse but in a teoricall manner, the Hypervisor is not part of the BSP for MX8QXP.

 

Regards

0 项奖励
回复

2,876 次查看
ripplejr
Contributor II

Hi,

Thanks for the help. I wanted to ask if there was any update on a potential fix?

0 项奖励
回复