Hi, is it possible to use other eink displays with the SABRE Platform for eReaders based on i.MX50? We are using the Eink mobius. Also, how many gpio are available? Thanks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi, is it possible to use other eink displays with the SABRE Platform for eReaders based on i.MX50? We are using the Eink mobius. Also, how many gpio are available? Thanks

1,059件の閲覧回数
galdolber
Contributor I

Hi, is it possible to use other eink displays with the SABRE Platform for eReaders based on i.MX50? We are using the Eink mobius. Also, how many gpio are available? Thanks

ラベル(2)
0 件の賞賛
返信
1 返信

885件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Gal

i.MX50 FSL software supports only panels found on MX508-EVK Based E-Book add-on Board

though other panels also may be supported (sw modifications are needed).

IMXEBOOKDC2 E-BOOK Exp Daghter Card

L2.6.35__11.04_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation 2011.04.

Regarding gpios, there are 6 GPIO modules (each 32bit), please read IMX50RM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信