Hi, i found my board w/ iMX6Q + PMIC cannot boot up, and the power of VDDARM_CAP and VDDCORE_CAP power issue: huge voltage drop while power on, from 1.1V down to 0.5V then up to 1.1V again. but the input power VDDARM and VDDCORE are stable.what's wrong?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi, i found my board w/ iMX6Q + PMIC cannot boot up, and the power of VDDARM_CAP and VDDCORE_CAP power issue: huge voltage drop while power on, from 1.1V down to 0.5V then up to 1.1V again. but the input power VDDARM and VDDCORE are stable.what's wrong?

1,144 次查看
nealli
Contributor I

and i cannot use OTG to upgrade the firmware, because PC cannot recogenize the OTG port. anybody can help?

0 项奖励
回复
3 回复数

1,079 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Li

please check Chapter 8 Avoiding Board Bring-up Problems

i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,079 次查看
nealli
Contributor I

i also measured these power PI on SDB CRB, and same issue with my board.

and if i power on VDDHIGH_IN before VDDCORE and VDDARM, then this issue disappeared.

please double check with CRB.

0 项奖励
回复

1,079 次查看
igorpadykov
NXP Employee
NXP Employee

right, recommended to power VDDHIGH_IN before other power supplies,

immediately after VDD_SNVS_IN, as it is done on i.MX6QP SPF-28857

with MMPF0100F9.

~igor

0 项奖励
回复