Hi, could you please provide the Differential Input Voltage value VID (min, max) and Differential Output Voltage value VOD (min, max) for MCIMX6Q6AVT10AD processor for HDMI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi, could you please provide the Differential Input Voltage value VID (min, max) and Differential Output Voltage value VOD (min, max) for MCIMX6Q6AVT10AD processor for HDMI

950 次查看
muralikrishna
Contributor I

Hi,

           could you please provide the Differential Input Voltage value VID (min, max) and Differential Output Voltage value VOD (min, max) for MCIMX6Q6AVT10AD processor for HDMI & DDR3L interfaces.

标签 (1)
0 项奖励
回复
1 回复

867 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Murali

i.MX6 has not HDMI input, so input HDMI characteristics are not specified.

As for output: VSWING= 400(min.) - 600(max.)  mV as given in

Figure 57 Driver Definitions, Table 63 Electrical Characteristics IMX6DQCEC

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复