Hi all,请帮忙解答问题:i.MX280的GPIO电平是1.8V还是3.3V?or 任意GPIO均可单独配置这两种电平? Thanks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi all,请帮忙解答问题:i.MX280的GPIO电平是1.8V还是3.3V?or 任意GPIO均可单独配置这两种电平? Thanks

Jump to solution
1,145 Views
alyssawu
Contributor I

Hi all,

请帮忙解答问题:i.MX280的GPIO电平是1.8V还是3.3V?or 任意GPIO均可单独配置这两种电平?

Thanks

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
996 Views
igorpadykov
NXP Employee
NXP Employee

Q: Please help answer questions: i.MX280 the GPIO level is 1.8V or 3.3V? GPIO can be configured

individually or in any of these two levels? [translated by Google]

Hi alyssa

please refer to sect.9.2.2.2 Pin Voltage Selection MCIMX28RM  :

Each GPIO (non-EMI) pin can be programmed to operate at either 1.8 V or 3.3 V by setting

the bit corresponding to that pin in one of the HW_PINCTRL_DRIVEx registers. The EMI

pins are capable of running at 1.5/1.8 V depending on the EMI_VDDIO voltage.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

如果这个职位回答你的问题,请点击正确答案按钮。谢谢![由谷歌翻译]

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
996 Views
alyssawu
Contributor I

坐等回复啊.............:smileyconfused:

0 Kudos
Reply
997 Views
igorpadykov
NXP Employee
NXP Employee

Q: Please help answer questions: i.MX280 the GPIO level is 1.8V or 3.3V? GPIO can be configured

individually or in any of these two levels? [translated by Google]

Hi alyssa

please refer to sect.9.2.2.2 Pin Voltage Selection MCIMX28RM  :

Each GPIO (non-EMI) pin can be programmed to operate at either 1.8 V or 3.3 V by setting

the bit corresponding to that pin in one of the HW_PINCTRL_DRIVEx registers. The EMI

pins are capable of running at 1.5/1.8 V depending on the EMI_VDDIO voltage.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

如果这个职位回答你的问题,请点击正确答案按钮。谢谢![由谷歌翻译]

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
996 Views
alyssawu
Contributor I

Hi igro,

Thanks for your reply.

Are you the freescale Employee?:smileywink:

0 Kudos
Reply