Hi, Im trying to use ETM from IMX 6Solox which i used from Zynq zc706 board.
But something went wrong. so IMX 6Solox doesn't get result of ETM tracing. on ETB Buffer.
Are there any ppl who got some any idea about my problem???
thx.
Hi,
If you are having troubles with Zynq ZC706 board, you should contact Xilinx support. Regarding ETM, its availability depends of the kind of JTAG access allowed and used debug probe (like ARM DSTREAM).
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
Hey Carlos. Thanks for your help.
I don have problem in Zynq zc706 board.
Im trying to use ETB buffer which is already inside of the IMX6sx board to check my PTM traces which should be written in ETB. That is why im trying to check the packet from the ETB buffer.
But unfortunately, something went wrong. Is there any way i can check the ptm trace without using JTAG or debug probe??