Hi, Could you please provide the IBIS model for MCIMX6Q6AVT10AD Processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, Could you please provide the IBIS model for MCIMX6Q6AVT10AD Processor

664 Views
muralikrishna
Contributor I

Hi,

Could you please provide the IBIS model for MCIMX6Q6AVT10AD Processor

Regards

Murali

0 Kudos
Reply
1 Reply

584 Views
igorpadykov
NXP Employee
NXP Employee

Hi Murali

i.MX6Q ibis model is located on link below

IMX6_DQ_IBIS : i.MX 6Quad and i.MX 6Dual IBIS File.

Size (K): 17035 Format: zip Rev #: 1.4 Modified: 12/3/2013


"Simulation and Models-IBIS (1) "

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply