Help with the problem to download uboot img by dd commnd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help with the problem to download uboot img by dd commnd

1,953 Views
transfer168
Contributor I

We want to use dd command to download uboot image instead of MFGtool to fast debugging process as the following Freescale  documents  mention:

Although the steps can be finshed, the uboot remains the same as before. We made a special printf flag to verify this.  However, with the same uboot image, MFGtool can update it without problem.  Is there any extra step has to be done ?  security etc.

By the way, there is NO problem with dd recocery Image.

We are testing sabresd_6dq for smart devices and anroid 4.4.3.

Thanks for any suggestion.

1:

https://community.freescale.com/docs/DOC-95015

2: Android user guide:

  1. 4.1.3 Downloading images with dd utility

The Linux utility "dd" on Linux computer can be used to download the images into the MMC/SD/TF card.

Before downloading, ensure that your MMC/SD/TF card partitions are created as described in Storage partitions.

All partitions can be recognized by the Linux computer. To download all images into the card, use the commands below:

Download the U-Boot image:

# sudo dd if=u-boot.imx of=/dev/sdx bs=1K seek=1; sync

Download the boot image:

# sudo dd if=boot.img of=/dev/sdx1; sync

Download the Android system root image:

# sudo dd if=system.img of=/dev/sdx5; sync

Download the Android recovery image:

# sudo dd if=recovery.img of=/dev/sdx2; sync

Labels (3)
Tags (1)
0 Kudos
Reply
3 Replies

1,431 Views
b36401
NXP Employee
NXP Employee

The commands seems to be correct. Do the card have right partitions? Are you using right "x" letter there?

If you are unsure about the commands you can make one single TF card using MFGtool

then make sure that it works fine and then make its image:

# sudo dd if=/dev/sdx of=OSimage bs=1024k

And then you can simply burn the image to fresh cards:

# sudo dd if=OSimage of=/dev/sdx bs=1024k

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,431 Views
transfer168
Contributor I

Hi Victor,

Thanks for your reply.

During this debugging, we use EMMC on device which is /dev/block/mmcblk3 (android). After android booting successfully, we confirm this by mount command output.

We want this dd way to avoid too many hardwre setting changes like dip switch, usb cables plugging etc. After uboot is built, then adb pushes it to device, then dd updates it.  This way will save lot of time comparing to MFGtool method.

Thanks for any more suggestion.

Have a nice day,

Tony

0 Kudos
Reply

1,432 Views
transfer168
Contributor I

The sabresd_6dq console log is attached here:

The log shows that bs=1k is just treat as bs=1. But this correction does not fix the problem.

/worng command mentioned in doc:

dd if=u-boot-imx6q.imx of=/dev/block/mmcblk3 bs=1K seek=1; sync                                 <

392192+0 records in

392192+0 records out

392192 bytes transferred in 3.848 secs (101920 bytes/sec)

/Correct command:

dd if=u-boot-imx6q.imx of=/dev/block/mmcblk3 bs=1024 seek=1; sync                  <

383+0 records in

383+0 records out

392192 bytes transferred in 0.010 secs (39219200 bytes/sec)

root@sabresd_6dq:/data # sync

root@sabresd_6dq:/data # ls -l

drwxrwx--x system   system            1970-01-01 00:00 app

drwx------ root     root              1970-01-01 00:00 app-asec

drwxrwx--x system   system            1970-01-01 00:00 app-lib

drwxrwx--x system   system            1970-01-01 00:00 app-private

drwx------ system   system            1970-01-02 00:00 backup

lrwxrwxrwx root     root              1970-01-01 00:00 bugreports -> /data/data/com.android.shell/files/bugreports

drwxrwx--x system   system            1970-01-02 00:01 dalvik-cache

drwxrwx--x system   system            1970-01-02 00:00 data

drwxr-x--- root     log               1970-01-01 00:00 dontpanic

drwxrwx--- drm      drm               1970-01-02 00:00 drm

drwxr-x--x root     root              1970-01-01 00:00 local

drwxrwx--- root     root              1970-01-01 00:00 lost+found

drwxrwx--- media_rw media_rw          1970-01-02 00:00 media

drwxrwx--- mediadrm mediadrm          1970-01-01 00:00 mediadrm

drwxrwx--t system   misc              1970-01-01 00:00 misc

drwx------ root     root              1970-01-02 00:03 property

drwxrwx--x system   system            1970-01-01 00:00 resource-cache

drwx--x--x system   system            1970-01-01 00:00 security

drwxr-x--- root     shell             1970-01-01 00:00 ssh

drwxrwxr-x system   system            1970-01-02 00:03 system

-rwxrwxrwx root     root       392192 2015-09-04 20:35 u-boot-imx6q.imx

drwx--x--x system   system            1970-01-01 00:00 user

root@sabresd_6dq:/data # request_suspend_state: sleep (0->3) at 383982400378 (1970-01-02 00:09:16.350279711 UTC)

active wake lock gadget

active wake lock PowerManagerService.Display

active wake lock PowerManagerService.WakeLocks

mma enable setting inactive

root@sabresd_6dq:/data # ls -l /dev/block/mmc*

brw------- root     root     179,   0 1970-01-02 00:03 mmcblk2

brw------- root     root     179,   8 1970-01-02 00:03 mmcblk3

brw------- root     root     179,  16 1970-01-02 00:03 mmcblk3boot0

brw------- root     root     179,  24 1970-01-02 00:03 mmcblk3boot1

brw------- root     root     179,   9 1970-01-02 00:03 mmcblk3p1

brw------- root     root     259,   2 1970-01-02 00:03 mmcblk3p10

brw------- root     root     179,  10 1970-01-02 00:03 mmcblk3p2

brw------- root     root     179,  11 1970-01-02 00:03 mmcblk3p3

brw------- root     root     179,  12 1970-01-02 00:03 mmcblk3p4

brw------- root     root     179,  13 1970-01-02 00:03 mmcblk3p5

brw------- root     root     179,  14 1970-01-02 00:03 mmcblk3p6

brw------- root     root     179,  15 1970-01-02 00:03 mmcblk3p7

brw------- root     root     259,   0 1970-01-02 00:03 mmcblk3p8

brw------- root     root     259,   1 1970-01-02 00:03 mmcblk3p9

brw------- root     root     179,  32 1970-01-02 00:03 mmcblk3rpmb

dd if=u-boot-imx6q.imx of=/dev/block/mmcblk3 bs=1K seek=1; sync                                 <

392192+0 records in

392192+0 records out

392192 bytes transferred in 3.848 secs (101920 bytes/sec)

dd if=u-boot-imx6q.imx of=/dev/block/mmcblk3 bs=1024 seek=1; sync                  <

383+0 records in

383+0 records out

392192 bytes transferred in 0.010 secs (39219200 bytes/sec)

root@sabresd_6dq:/data #

root@sabresd_6dq:/data #

root@sabresd_6dq:/data #

root@sabresd_6dq:/data # sync

root@sabresd_6dq:/data #

power off ->on

=====> A flag is set to verify the new uboot image in log output:

Version ID:009BBA -----> :check_and_clean: reg 0, flag_set 0

But the results indicate the uboot image had not been updated by this way. But MFGtool can update the same uboot image correctly.

U-Boot 2014.04-08639-ge5ef3e4-dirty (Sep 04 2015 - 13:18:46)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 31 C, calibration data: 0x5924f87d

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

Found PFUZE100 deviceid=10,revid=11

Version ID:009BBA -----> :check_and_clean: reg 0, flag_set 0

Fastboot: Normal

flash target is MMC:2

Bad partition index:1 for partition:boot

Bad partition index:2 for partition:recovery

Bad partition index:5 for partition:system

Bad partition index:8 for partition:misc

Net:   FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  0

booti mmc2

booti: version:006CCC-------first check boot count in misc:0

------>just before reading booti partition: boot

booti: bad boot image magic

fastboot is in init......USB Mini b cable Connected!

fastboot initialized

USB_SUSPEND

USB_RESET

USB_PORT_CHANGE 0x4

USB_RESET

USB_PORT_CHANGE 0x4

0 Kudos
Reply