Help to decipher capacitor and inductor in schematic smd(pico-imx7d SOM)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help to decipher capacitor and inductor in schematic smd(pico-imx7d SOM)

977 次查看
neuberfran
Contributor IV

hI,

Screenshot_20200119-114156_Instagram.jpg

I need to know the name of this capacitors (on the L5 inductor side). My question (as schematic of the PMIC in the link below) is that in the U4B pmic figure there are 4.7U/10V/X5R-C2 and 0.1U/16V/X5R-C1 on the left side and 22U/6.3V/ X5R-C2 on the right side . Which one are the photo capacitors?

LINK:

nxp - Google Drive 

0 项奖励
回复
1 回复

877 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi NEUBER,

   pico-imx7d SOM  board is not designed by NXP, but Technexion. The board we released is MCIMX7D-SabreSDB, so if you want to know more information about these capacitors, you will have to check it's design files of PCB Layout.

   We don't have the design files of  pico-imx7d SOM, so I have no way to help you check it.

    The bettery way for you is to contact Technexion FAE or engineers.

Have a nice day!

BR,

Weidong

0 项奖励
回复