Hi guys,
I hope there is someone that can help me with an digital cockpit integration on a classic car.
Hi have all the TFT screens and MCIMX6QPAICPU3 - i.MX 6 Quad Plus SABRE Automotive Platform CPU Card.
I do understand that more hardware is needed, but would like to work closely with an experienced operator to help me put this all together.
I am based in Melbourne Australia, if their is someone near me would be preferable but not necessary.
I hope to hear from someone soon, even if it is to recommend someone.
Here is a link of what I would like to accomplish.
https://www.youtube.com/watch?v=KrCPQ55m_RM <https://www.youtube.com/watch?v=KrCPQ55m_RM
Thank you
Hi Maurice
one can look at documentation on that board
SABRE|Automotive-Infotainment|i.MX6|NXP
Schematics (5)
Design files for i.MX 6QuadPlus CPU3 Card with AVB
SABRE|Automotive-Infotainment|i.MX6|NXP
As mentioned on p.17 schematic parallel display is compatible
7" 800 x 480 LCD and software driver available from Boundary Devices.
Configuring i.MX6 boards for different screens - Boundary Devices
Other lcds are supported in NXP BSPs described on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------