Hello! At LAY-28617_C2 PCB, I want to use NAND(U302) to run the operating system, but Position conflict between R324 and U302,R324 connects the data pins of the nand(U302),how to use nand?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello! At LAY-28617_C2 PCB, I want to use NAND(U302) to run the operating system, but Position conflict between R324 and U302,R324 connects the data pins of the nand(U302),how to use nand?

528 Views
2659332355
Contributor I

Hello! At LAY-28617_C2  PCB, I want to use NAND(U302) to run the operating system, but Position conflict between R324 and U302,R324 connects the data pins of the nand(U302),how to use nand?

0 Kudos
Reply
1 Reply

443 Views
igorpadykov
NXP Employee
NXP Employee

Hi sasa


Hi sasa


for nand usage one can look at

How-To use NAND boot on i.MX6UL EVK board

How-To use NAND boot on i.MX6UL EVK board 

and sect.2.8 NAND flash i.MX 6UltraLite EVK Board Hardware User's Guide on link

https://www.nxp.com/imx6ul  --> Documentation Tab


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply