Hi tahi
for i.MX6 Linux please read L3.0.35_4.1.0_LINUX_DOCS
L3.0.35_4.1.0_ER_SOURCE_BSP
: i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code
Also you may wish to check bare metal tests
i.MX 6Series Platform SDK
: Bare-metal SDK for the i.MX 6 series
Yes you can use HDMI to VGA converters, note VGA is analog interface while HDMI is digital.
Probably it is better to use true (genuine) HDMI monitor.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------