Having trouble with network connectivity when using multiple Ethernet interfaces in NXP i.MX 8M plus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Having trouble with network connectivity when using multiple Ethernet interfaces in NXP i.MX 8M plus

1,426 次查看
Kiruthik-15
Contributor I

Hello Everyone,

I'm experiencing network connectivity issue , I'm unable to ping when using multiple Ethernet interfaces .

 

0 项奖励
回复
5 回复数

1,315 次查看
pengyong_zhang
NXP Employee
NXP Employee

HI @Kiruthik-15 

I have not do any change on my site, just use the default BSP code.

Because you sail "This occurs despite the laptop being connected to the internet via Wi-Fi" you should check your vpn.

B.R

 

 

 

0 项奖励
回复

1,354 次查看
pengyong_zhang
NXP Employee
NXP Employee

HI @Kiruthik-15 

i try your issue on my site, there is no problem occur on my site. Have you check if your network can access 8.8.8.8? 

pengyong_zhang_0-1725502812387.png

 

B.R 

0 项奖励
回复

1,345 次查看
Kiruthik-15
Contributor I

Hi Pengyong_zhang,

May I know what steps you have followed and if it's possible may i know which image you have used for the sdk.

 

B.R

0 项奖励
回复

1,336 次查看
Kiruthik-15
Contributor I
I think its based on routing preference
when the route eth0 is initially up then this issue is present .
Could you check , from my understanding i think this is due to routing (not sure) , please correct me if im wrong
0 项奖励
回复

1,405 次查看
Kiruthik-15
Contributor I
In the EVK , the ETH0 is able to ping camera and ETH1 is able to ping laptop . But However, when I attempt to ping an external IP address (e.g., 8.8.8.8) from the NXP i.MX MPlus Board, the request times out. This occurs despite the laptop being connected to the internet via Wi-Fi.
0 项奖励
回复