Having a problem with JTAG in IMX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Having a problem with JTAG in IMX6Q

1,040 Views
alielseddeek
Contributor II

Dear All,

I was trying to connect JTAG (DS-5) to my IMX6Q but I didn't succeed in making a working connection.

So, I wanted to know which signals that are necessary as I connected the VDD_SNVS_IN, VDD_HIGH_IN, VDDARM_IN ,VDDSOC_IN, and POR_B to power up.

Regarding the connections of the JTAG, I connected JTAG_TCK, JTAG_TDI, JTAG_TDO, JTAG_TMS, and JTAG_TRSTB in addition to VDD and ground of course.

Am I missing something else?

Thanks in advance

Best regards
Ali Elseddeek

Labels (1)
1 Reply

888 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ali

all processor power supplies should be provided according to datasheet,

with (probably) exception given in sect.2.8 Unused analog interfaces

i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

For jtag connections one can look at sect.2.6 JTAG signal termination

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------