Hi Community,
I'm using Yocto project imx-4.9.11_1.0.0_ga and I use i.MX6 sabre-SD Quad as my platform.
I use below Distro and build image with below commands.
Compiler is success and I got fsl-image-qt5-imx6qsabresd-20181126013844.rootfs.tar.bz2 in the path of build-wayland-q/tmp/deploy/images/imx6qsabresd.
After I burn new root file system and zimage and module, logo could show on panel but when get into system there is no desktop showing.
I try to run my application with "./application -platform wayland" then will result failed like below content.
Failed to create display (No such file or directory)
I also tried to use eglfs and wayland-egl, they all reply the same error as wayland.
Did I miss anything?
How can I solve this problem?
Thanks in Advanced!
解決済! 解決策の投稿を見る。
Bio_TICFSL 留言:
Hi tsung
You might try to burn to .sdcard image.
Regards
Thanks for your reply.
I rebuild it and it works.
I think there is something wrong when I bitbake it.
But here is another condition.
I will open the other thread asking for help.
Thanks!
Hi tsung
You might try to burn to .sdcard image.
Regards
Bio_TICFSL 留言:
Hi tsung
You might try to burn to .sdcard image.
Regards
Thanks for your reply.
I rebuild it and it works.
I think there is something wrong when I bitbake it.
But here is another condition.
I will open the other thread asking for help.
Thanks!