Have GPU/VPU power gating been supported by i.MX6 current BSP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Have GPU/VPU power gating been supported by i.MX6 current BSP?

Jump to solution
702 Views
satoshishimoda
Senior Contributor I

Hi community,

I havea a question about i.MX6DQ power gating.

Please see page. 59 in AN4579, it says "Support for this feature is planned for the next BSP Release".

I think "next BSP Release" mentions L3.0.35_1.1.1, so all current BSPs (Linux & Android) have supported GPU/VPU power gating already.

Is this correct?

Best Regards,

Satoshi Shimoda

Tags (3)
0 Kudos
1 Solution
486 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes correct, one can look at linux gpc.c and  Chapter  General Power Controller (GPC) RM

Linux/arch/arm/mach-imx/gpc.c - Linux Cross Reference - Free Electrons

Best regards

igor
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
487 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes correct, one can look at linux gpc.c and  Chapter  General Power Controller (GPC) RM

Linux/arch/arm/mach-imx/gpc.c - Linux Cross Reference - Free Electrons

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos