Has the imx28 revisions been updated for ERR010873

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has the imx28 revisions been updated for ERR010873

Jump to solution
1,346 Views
liuxing
Contributor II

Hi All,

   We have a big concern about the ERR010873. We want a clear information about if imx28 ROM code has been updated for it.Is the uboot patch enough for preventing  hacker attacks?

Labels (1)
0 Kudos
1 Solution
1,275 Views
joanxie
NXP TechSupport
NXP TechSupport

Rev 1.3 means imx28 IC version, you can check the part number, the last ‘“c” in the part number means MCIMX28 Revision 1.3

View solution in original post

0 Kudos
4 Replies
1,275 Views
joanxie
NXP TechSupport
NXP TechSupport

as I known, 1.3 version is fixed the ERR010873, so try to updata to the new version

 

0 Kudos
1,275 Views
liuxing
Contributor II

Hi Joan,

      Thanks a lot for your reply!

       I'm not sure if you misunderstand my question.

       I mean the imx28x IC version to fix the ERR010873.As I know,the rom code in the IC can't be updated.

0 Kudos
1,276 Views
joanxie
NXP TechSupport
NXP TechSupport

Rev 1.3 means imx28 IC version, you can check the part number, the last ‘“c” in the part number means MCIMX28 Revision 1.3

0 Kudos
1,275 Views
liuxing
Contributor II

Hi,

  Another question,Is the secure boot can enabled without HABv4?

Does the following description means it can enable encrypted boot feature only?

Secure Boot
A key feature of the i.MX28 ROM is the ability to perform a secure boot. This is
supported by
• The encrypted boot feature and
• The High Assurance Boot (HAB)
These are independent features and are not dependent on each other.

0 Kudos