Has software modification in EB803 been applied to Yocto BSP (L3.10.17_1.0.0-ga)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Has software modification in EB803 been applied to Yocto BSP (L3.10.17_1.0.0-ga)?

ソリューションへジャンプ
1,302件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ Yocto BSP (L3.10.17_1.0.0-ga).

Please see EB803(http://cache.freescale.com/files/microcontrollers/doc/eng_bulletin/EB803.pdf),  it says some modifications are needed for L3.0.35_4.1.0 if use rev.1.3 chip.

Then, how about for L3.10.17_1.0.0-ga?

Same modifications are needed same as L3.0.35_4.1.0? or has L3.10.17_1.0.0-ga been applied the modifications?

Best Regards,

Satoshi Shimoda

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 解決策
1,170件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, the software modifications, mentioned in EB803, been applied to Yocto BSP (L3.10.17_1.0.0-ga)

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,171件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes, the software modifications, mentioned in EB803, been applied to Yocto BSP (L3.10.17_1.0.0-ga)

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信