Has software modification in EB803 been applied to Yocto BSP (L3.10.17_1.0.0-ga)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has software modification in EB803 been applied to Yocto BSP (L3.10.17_1.0.0-ga)?

Jump to solution
1,211 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ Yocto BSP (L3.10.17_1.0.0-ga).

Please see EB803(http://cache.freescale.com/files/microcontrollers/doc/eng_bulletin/EB803.pdf),  it says some modifications are needed for L3.0.35_4.1.0 if use rev.1.3 chip.

Then, how about for L3.10.17_1.0.0-ga?

Same modifications are needed same as L3.0.35_4.1.0? or has L3.10.17_1.0.0-ga been applied the modifications?

Best Regards,

Satoshi Shimoda

Labels (3)
Tags (1)
0 Kudos
Reply
1 Solution
1,079 Views
Yuri
NXP Employee
NXP Employee

Yes, the software modifications, mentioned in EB803, been applied to Yocto BSP (L3.10.17_1.0.0-ga)

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,080 Views
Yuri
NXP Employee
NXP Employee

Yes, the software modifications, mentioned in EB803, been applied to Yocto BSP (L3.10.17_1.0.0-ga)

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply