Has errata fixed in enhanced EPDC of i.MX6SLL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Has errata fixed in enhanced EPDC of i.MX6SLL?

ソリューションへジャンプ
1,072件の閲覧回数
torus1000
Contributor V

Hi, 

I compared two errata(IMX6SLLCE.pdf and IMX6SLCE.pdf) then found known EDDC errata ERR005313 disappeared.
I guess errata was fixed but I couldn't find any descriptions in "i.MX 6SLL Migration Guide: AN11988.pdf".

Has the errata ERR005313 been already fixed?

If someone know it, please let me know.

ERR005313 EPDC: Incorrect data fetched when the buffer update width is 2048 pixels or greater

Description:
When sending an image update to a high resolution panel with an image buffer width ≥ 2048 pixels,
the EPDC module fetches incorrect data because an internal address register is incorrectly
truncated.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
907件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Torus1000,

I confirmed that this erratum was fixed since i.MX6SL and it is also fixed on the i.MX6SLL.

I hope this helps!

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
908件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Torus1000,

I confirmed that this erratum was fixed since i.MX6SL and it is also fixed on the i.MX6SLL.

I hope this helps!

Regards,

0 件の賞賛
返信