Has anyone tried Yocto 3.10.17_1.0.0 GA u-boot v2013.04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has anyone tried Yocto 3.10.17_1.0.0 GA u-boot v2013.04

668 Views
rajniks
Contributor I

Hello,

I have setup a Yocto cross-compiler tool chain and I am running the deploy command for u-boot without doing any changes for SABRESDB card. I am flashing the u-boot binary on the SD card but the board doesn't boot. I have taken the u-boot-mx6q-sabresd.bin from MFG tool which is U-Boot 2009.08 version and works perfectly fine.

Has anyone tried the latest Freescale u-boot v2013.04 on the SabreSDB board. If yes please let me know if there is something I am missing here in order to compile the u-boot.

Labels (3)
0 Kudos
1 Reply

424 Views
Yuri
NXP Employee
NXP Employee

  It is needed to use u-boot-imx in Yocto.
In particular,  from documentation :
Enter the following command to copy the U-Boot image to the SD/MMC card,
where the U-Boot image can be any of the following:

• u-boot-imx6dlsabreauto_sd.imx

• u-boot-imx6slevk_sd.imx

• u-boot-imx6dlsabresd_sd.imx

• u-boot-imx6solosabreauto_sd.imx

• u-boot-imx6qsabreauto_sd.imx

• u-boot-imx6solosabresd_sd.imx

• u-boot-imx6qsabresd_sd.imx

$ sudo dd if=<U-Boot image> of=/dev/sdb bs=512 seek=2 conv=fsync


The first 1 KB of the SD/MMC card, that includes the partition table, will be preserved.

The i.MX 6 SABRE-SD Linux delivery package contains the following
U-Boot boot loader binary:


i.MX 6Quad SABRE-SDB and i.MX 6Quad SABRE-SDP:

• u-boot-imx6qsabresd.imx (SD/MMC)

• u-boot-imx6qsabresd-sata.imx (SATA)


i.MX 6DualLite SABRE-SDP:

• u-boot-imx6dlsabresd.imx (SD/MMC)


i.MX 6DualLite SABRE-SDP (Solo Emulation):

• u-boot-imx6solosabresd.imx (SD/MMC)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos