HY4635 touch controller not responding properly

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HY4635 touch controller not responding properly

3,309 次查看
karthikssk
Contributor I

Hi,

I am using a 7" LCD (800*480)display(RGB interface) with cap touch (I2C interface) and the touch controller used is HY4635 and IMX6 SOLO processor is used. So the response of the touch is not very accurate and when the values are read in terminal window most of the time it shows wrong (X,Y) values like out of bound. 

Only some times there is the response . we cannot  do the drag operation but once in a while just single touch will respond that to very slowly . 

Can anyone please suggest whats the issue?

Any driver changes that need to be done ?

标记 (1)
0 项奖励
回复
1 回复

2,380 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Karthik

one can test with linux driver provided by HY4635 vendor

http://www.hycontek.com/wp-content/uploads/Linux_driver_sample_code.zip 

and try to calibrate using guidelines on

Tweaking Froyo for Nitrogen Part 1: touch support - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复