HT mode is not supported by imx6ul

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HT mode is not supported by imx6ul

2,452 Views
surendradhobale
Contributor III

Hello,

   While reading the imx6ul referance manual, observed HT mode is not supported by imx6ul. ( chapter 20 , ECSPI section)

This is 1 bit field  ECSPIx_CONREG register.

{ Hardware Trigger Enable. This bit is used in master mode only. It enables hardware trigger (HT) mode.

Note, HT mode is not supported by this product.

0 Disable HT mode.

1 Enable HT mode. }

For what purpose this bit is used ?  Is this related to native chip select, as native chip select driven by hardware only.

 

Labels (3)
0 Kudos
Reply
3 Replies

2,095 Views
Yuri
NXP Employee
NXP Employee

Hello,

    ECSPI module (IP) in i.MX6 does not have HT implemented, since 

 there are no corresponding trigger inputs.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,095 Views
hrishikesh23
Contributor I

Hi Yuri,

Thanks for your reply.

But is this trigger some how associated with Native chip select.

0 Kudos
Reply

2,095 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply