HOW to use sdma channel to transfer data for uart?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HOW to use sdma channel to transfer data for uart?

3,990件の閲覧回数
jingyangxie
Contributor V

I used imx6qsabread board,can anyone tell me how to use sdma channel to transfer data for uart or give me an example

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,572件の閲覧回数
frank_zhang
NXP Employee
NXP Employee

Hi jingyang,

     It looks like common UART has used SDMA to transfer data. You can refer to Appendix A SDMA Scripts in i.MX6RM.Thank you!

Best Regards,

Frank

0 件の賞賛
返信

3,572件の閲覧回数
jingyangxie
Contributor V

HI,Frank

      thaks for your answer,but I still can't understand usage of sdma for uart,can you give me an example ?

0 件の賞賛
返信

3,571件の閲覧回数
frank_zhang
NXP Employee
NXP Employee

Hi jingyang,

       For the SDMA usage of Linux UART driver, you can refer to chapter 47 of i.MX Linux RM. I paste some paragraphs as below.

     Each UART can be configured to use DMA for the data transfer by enabling the DMA
channel in the DTS file.
     The driver requests two DMA channels for the UARTs that need DMA transfer. On a
receive transaction, the driver copies the data from the DMA receive buffer to the TTY
Flip Buffer 

       While using DMA to transmit, the driver copies the data from the UART transmit buffer
to the DMA transmit buffer and sends this buffer to the DMA system. For more
information, see the Linux documentation on the serial driver in the kernel source tree.

       Also you can check the driver <Yocto_BuildDir>/linux/drivers/tty/serial/imx.c and the related dts file, Thank you!

Best Regards,

Frank

3,571件の閲覧回数
jingyangxie
Contributor V

Hi,Frank

    I  read the chapter and check the driver,the driver supports DMA ,but how can I use this in an application?

could you give me an source code example?

0 件の賞賛
返信

3,571件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

From the application layer, any application doesn't know about the hardware detail including using or not using DMA.

That is why need different layer for  software and OS. One application can run under the different platform.

The different is the speed and the CPU loading if it is using or not using DMA.

3,572件の閲覧回数
frank_zhang
NXP Employee
NXP Employee

Hi jingyang,

    Per my understanding, if you enable the tx and rx dma channels in the dts file(it should aready be enabled by default), it can enable SDMA support for UART. Do you need the sample code for the sdma mem2mem application? You can refer to  https://community.nxp.com/message/862063?commentID=862063#comment-862063 

    Thank you!

Best Regards,

Frank

0 件の賞賛
返信