Hi, I would like to apply PREEMPT-RT patch for i.mx6ul board in yocto.
However I was not able to do it, so I would like you to tell me the way.
Right now I use yocto 2.0 (Jethro).
I found linux-yocto-rt_4.1.bb file in sources/poky/meta/recipes-kernel/linux.
After bitbake I checked $ uname -a, but it did not say PREEMPT RT.
I think I would be able to make preempt rt kernel image if I could correctly apply linux-yocto-rt_4.1.bb.
How can I apply the recipe ? Or if there are other way to make preempt rt kernel image, would you tell me the way please?
And I found a readme file which says "In order to build the image with the linux-yocto-rt kernel, be sure to include the following line in your local.conf, bblayers.conf, or your $MACHINE.conf.
PREFERRED_PROVIDER_virtual/kernel = "linux-yocto-rt" " in sources/poky/meta/recipes-rt.
So I added the line in my bblayers.conf and local.conf, but I could not make rt image.
In the readme file, it also says about core-image-minimal. It means that we can use linux-yocto-rt only in core-image-minimal image? I would like to use other image.
Furthermore, I found linux-fslc-mx6-rt_3.14-1.0.x.bb in sources/meta-fsl-arm/receipes-kernel/linux.
Does it have relation?
Thank you for reading.
I am looking forward to your reply.
Best regards,
Hiro
Solved! Go to Solution.
Hi Hiro
nxp bsps do not support rt, linux-fslc-mx6-rt_3.14 is community version of bsp
so this may be posted on meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
difference between nxp official bsps and community bsps is described on
https://community.freescale.com/message/402940#402940
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Hiro
nxp bsps do not support rt, linux-fslc-mx6-rt_3.14 is community version of bsp
so this may be posted on meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
difference between nxp official bsps and community bsps is described on
https://community.freescale.com/message/402940#402940
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor
I am so sorry for not replying your post. I had a login problem...
Thank you for your answer.
I will use the mailing list.
Best regards
Hiro