HMDI display shutdown when wayland loaded

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HMDI display shutdown when wayland loaded

1,189 Views
x10
Contributor V

Hardware: iMX8MM-EVK + MIPI-DSI to HDMI

Platform: uboot2017 + Linux-4.14.98_2.0.0 from yocto 2.0

Description:

Display is okay with uboot up, and display setting through commandline (video=1280x720-32@60e) is fine during kernel loading. The "OpenEmbedded" loading screen can been seen, and then display is shutdown without wayland desktop. 

More than three LCD monitors are used for testing, only one monitor can display wayland desktop. 

It's appreciated for any comments and hits. Thanks in advance

Best Regards

Cheng Shi

www.emtronix.com

Labels (1)
1 Reply

1,119 Views
x10
Contributor V

Problem fixed,it should add the following commandline

drm_kms_helper.edid_firmware=edid/your_edid.bin

instead of "video=..." to force display resolution.