HM5065 camera module with IMX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HM5065 camera module with IMX6SL

1,475 Views
vinothrajm
Contributor III

Hi,

Now i am working on the HM5065 camera module with IMX6SL. I can able to get the images from HM5065 camera module with IMX6SL in Android platform.

But the problem is that, the image is shaded by some (pink) colour.I also attached  the sample images are taken from  HM5065 camera module.

Kindly Give any suggestion to solve this issue

Regards,

vinothraj

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

1,128 Views
igorpadykov
NXP Employee
NXP Employee

Hi vinothraj

this looks like incorrect camera format, for

i.MX6SL one can look at SDK drivers/camera example

and unit tests pxp_v4l2_test in

http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply