dear expert :
now our product switch to imx8qxp c0 chip , we try to download c0 image in sdps , but when we run :
sdps: boot -f flash.bin
if show error HID(R) :LIBUSB_ERROR_TIMEOUT immediately , we captured usb bushound log , only follow log printed when run download cmd:
6.0 CTL 23 03 02 00 04 00 00 00 CLASS 30.1.0
6.0 CTL 23 01 02 00 04 00 00 00 CLASS 31.1.0
7.1 IN 10 . 32.1.0
6.0 CTL a3 00 00 00 04 00 04 00 CLASS 33.1.0
6.0 IN 03 05 04 00 .... 33.2.0
6.0 CTL 23 01 12 00 04 00 00 00 CLASS 34.1.0
6.0 CTL a3 00 00 00 04 00 04 00 CLASS 35.1.0
6.0 IN 03 05 00 00 .... 35.2.0
6 CMD 00 00 00 00 00 00 00 00 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 20 d5 b4 ad 09 c6 ff ff TEST UNIT READY 36.1.0(2)
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 36.1.32
00 00 00 00 00 00 00 00 13 00 08 02 53 65 54 6c e5 c6 0e 27 38 52 38 d7 b0 11 94 a8 09 c6 ff ff 36.1.64
70 ec 4c af 09 c6 ff ff 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 36.1.96
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 36.1.128
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 36.1.160
6 SSTS 00 pending 36.2.0
6.0 CTL 23 03 02 00 04 00 00 00 CLASS 38.1.0
then it show error and no other log print;
why this happened ? what should i do ?
thanks