hi
i used IMX8QM-MEK.
I downloaded SURROUND VIEW 3D 1.1 beta.zip from the NXP site.
It is testing with reference to SVARM and SVAUG pdf documents.
i used YOCTO sumo-4.14.98.
And I also referred to the site below.
https://www.wpgdadatong.com/cn/blog/detail?BID=B0742
However, if you run the next software, it will stop as follows.
cd Tools/CamCapture/
./capturing 1
and keyboard 'p' press
Randomly dying. (1-10 times) --> segment fault.
----- error
sh-4.4# ./capturing 1
Width = 1280 Height = 800
Image size = 2048000
Pixelformat YUYV
WxH@fps = 1280x800@30 Image size = 2048000
Segmentation fault (core dumped)
In addition, even if captured, the stored image is as follows.
Do I need a patch?
regards.