HELP ME DEBUG AND modify IMX6Q BOOT REGISTER???

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HELP ME DEBUG AND modify IMX6Q BOOT REGISTER???

894 Views
liuwan
Contributor I

IMX6Q  USE  4PCS  NT5CB256M16CP-DII as  DRAM,how to config imx6q's register  ,UBOOT FILE?

Labels (1)
0 Kudos
Reply
4 Replies

745 Views
igorpadykov
NXP Employee
NXP Employee

Hi liu

first please run ddr test

i.MX6/7 DDR Stress Test Tool V2.90 

DES-N1936 i.MX 6UltraLite DDR Tools Overview and Hardware Design Considerations.pdf 

use attached Porting Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

745 Views
liuwan
Contributor I

HI,IGO'

     I HAVE DONE  DDR STRESS TEST  MONTH AGO,most time have  problem  DQS test error,BUT if  write & read  a single address ,i found this  operation success,MAYBE  BLOCK read /write failed,how can  use softwaretool  can make sure the CHIP IMX6Q having solder problem,SO as  the two addr-pin have  conneted?or pretended solder? 

0 Kudos
Reply

745 Views
igorpadykov
NXP Employee
NXP Employee

for solder problems one can test with jtag and oscilloscope or inspect layout using x-ray screening.

0 Kudos
Reply

745 Views
liuwan
Contributor I

dear,

      i  found a  problem,when i  have  fourteen pcs BOARD,some  PCBS DDR DRESS TEST ,I CAN  read/write  single word (32bit) for single address,but  DDR dress test  some address write have wrong hex data,how to fine tune the register for writing  sequence in time?

0 Kudos
Reply